1.3.17.21 PDECx_COUNTERCompare1Set Function

C

bool PDECx_COUNTERCompare1Set ( uint16_t compare1 ) // x is instance of the peripheral and it is applicable only for devices having multiple instances of the peripheral.

Summary

Configures Compare 1 register value

Description

This function configures Compare 1 (CC1) register value.

Precondition

PDECx_COUNTERInitialize function must have been called first for the given channel.

Parameters

Param Description
compare1 Value to be set in Compare 1 register

Returns

true - If Compare 1 register set false - If Compare 1 register is not set

Example

PDEC_COUNTERInitialize();
PDEC_COUNTERStart();
PDEC_COUNTERCompare1Set(0x100);

Remarks

None.