1.6.10.1 EIC_Initialize Function

C

void EIC_Initialize (void);

Summary

Initializes given instance of EIC peripheral.

Description

This function initializes given instance of EIC peripheral of the device with the values configured in MHC GUI.

Precondition

MHC GUI should be configured with the right values.

Parameters

None.

Returns

None.

Example

EIC_Initialize();

Remarks

This function should only be called once during system initialization before any other EIC function is called.