1.9.18.4 SDMMCx_IsWriteProtected Function
C
/* x = SDMMC instance number */ bool SDMMCx_IsWriteProtected ( void )
Summary
Returns the write protect switch pin level.
Description
Returns the write protect switch pin level.
Precondition
SDMMCx_Initialize() must have been called first for the associated instance.
Parameters
None.
Returns
true - If the card is write protected.
false - If the card is write enabled.
Example
if (SDMMC1_IsWriteProtected() == false) { // Card is not write protected }
Remarks
None.