1.7.22.17 RTC_Timer32PeriodGet Function

C

uint32_t RTC_Timer32PeriodGet ( void )

Summary

Get 32-bit timer period Value.

Description

This function returns the 32-bit timer period value which used to compare with the current counter value. This value will match the value that was set using the RTC_Timer32CompareSet() function.

Precondition

RTC_Initialize must have been called for the associated RTC instance. The RTC peripheral should have been configured in 32-bit Timer Counter mode.

Parameters

None.

Returns

The current 32-bit timer period value.

Example

uitnt32_t period = 0;
RTC_Initialize();
RTC_Timer32CompareSet(0xFFF);

// period will have the same value is 0xFFF.
period = RTC_Timer32PeriodGet();

Remarks

None.