1.31.2.9 ADCx_WindowMonitorStatusGet Function
C
bool ADCx_WindowMonitorStatusGet( void );
Summary
Returns the status of the window monitor flag.
Description
This function checks whether ADC conversion result is within configured window thresholds.
Precondition
ADCx_Initialize() function must have been called first for the associated instance. Also conversion must have been started.
Parameters
None.
Returns
false - Result is outside configured window thresholds true - Result is within configured window thresholds
Example
bool windowMonitorStatus = false; ADC0_Initialize(); ADC0_ConversionStart(); windowMonitorStatus = ADC0_WindowMonitorStatusGet();
Remarks
This function is applicable only when window monitor mode is enabled.