1.12.9.3 EEPROM_PageErase Function
C
bool EEPROM_PageErase( uint32_t addr )
Summary
Erases one word in data EEPROM
Description
Erases one word in data EEPROM
Precondition
None
Parameters
Param | Description |
---|---|
addr | start address of the word to be erased |
Returns
Returns true on success false on error
Example
uint32_t i; uint32_t addr = 0; for ( i = 0; i < 4; i++ ) { result = EEPROM_PageErase( addr ); if (result == true) { addr = addr + 4; } }