1.17.6.12 DMAC_CRCRead Function
C
uint32_t DMAC_CRCRead( void )
Summary
DMA CRC read function
Description
Reads the generated DMA CRC value.
For some devices, It performs crc reverse and final xor operation based on setup parameters during DMAC_ChannelCRCSetup()
For some devices, when CRC-32 polynomial is used via CRCSetup, the final checksum read is bit reversed and complemented
Parameters
None
Returns
crc - Generated crc value
Example
Example of this function varies based on device family. Refer to the one which is applicable for the device being used.
DMAC_CRC_SETUP crcSetup = {0}; transfer_completed = false; uint32_t crc = 0; crcSetup.reverse_data_input = true; crcSetup.polynomial_length = 32; crcSetup.polynomial = 0x04C11DB7; crcSetup.non_direct_seed = 0x46AF6449; crcSetup.reverse_crc_output = true; crcSetup.final_xor_value = 0xFFFFFFFF; DMAC_ChannelCRCSetup(DMAC_CHANNEL_0, crcSetup); DMAC_ChannelTransfer(...); if (transfer_completed == true) { crc = DMAC_CRCRead(); }
DMAC_CRC_SETUP crcSetup = {0}; transfer_completed = false; uint32_t crc = 0; crcSetup.polynomial_type = DMAC_CRC_TYPE_32; crcSetup.seed = 0xFFFFFFFF; DMAC_ChannelCRCSetup(DMAC_CHANNEL_0, crcSetup); DMAC_ChannelTransfer(...); if (transfer_completed == true) { crc = DMAC_CRCRead(); }
Remarks
Once Read is done, DMAC_ChannelCRCSetup() has to be called again to setup the seed before performing DMA transfer for CRC generation.