3.45.19 Supply Controller (SUPC)

The Supply Controller (SUPC) controls the supply voltages of the system. The SUPC also generates the slow

clock by selecting either the low-power RC oscillator or the low-power crystal oscillator.

Using The Library

Configure the peripheral library using the MCC.

Library Interface

Supply Controller peripheral library provides the following interfaces:

Functions

NameDescription
SUPC_InitializeInitializes SUPC module of the device