9 Frame Replication and Elimination for Reliability (FRER)
Frame Replication and Elimination for Reliability (FRER), as specified in the IEEE 802.1CB-2017 standard, provides increased reliability (reduced packet loss rates) for a stream.
This is achieved by the following measures:
- Sequence numbering and replicating packets in the talker (source) end system and/or in relay systems in the network is called generation.
- Eliminating those replicates in the listener (destination) end system and/or in other relay systems is called recovery.

FRER is supported by Microchip’s SparX-5i and LAN9668 switch chips running IStaX software. There are differences between the two, which are explained in the subsequent sections.