9.1 Generating FRER using Web GUI
To generate FRER, perform the following steps:
- To enable VLAN hybrid on both Ingress and Egress ports, see Time Aware Shaper.
- Click TSN > Streams. The
Stream Configuration page opens.
Figure 9-2. Stream Configuration - To add a stream, click + .
- Click TSN > FRER.
The FRER Configuration page opens. On the configuration page, perform the
following:
- Press +.
- To set mode, in the Mode list, click Generation.
- Configure Instance, FRER VLAN, Ingress Stream List, and Egress Stream List, as shown in the following figure.
- To enable FRER, select the Enable check box.
- Click Save.
Figure 9-3. FRER Configuration