8.1 Configuring PSFP using Web GUI
To configure the PSFP, perform the following steps:
- To enable VLAN hybrid on both Ingress and Egress ports, see Time Aware Shaper.
- Click TSN >
Streams. The Stream Configuration
Overview page opens.
Figure 8-2. Stream Configuration Overview - To add a stream, click + .
- In the Stream
Configuration page, perform the following configuration:
- To set the Stream ID, type a suitable number in the Stream ID box.
- To add VLAN tags, configure the properties as shown in the following figure.
- To select the the port members (Ingress and Egress), select the appropriate Member check box.
- Click Save.
Figure 8-3. Stream Configuration
- Click TSN >
PSFP > Stream Filter. The
PSFP Stream Filter Configuraion page opens.
Figure 8-4. PSFP Stream Filter Configuration - Click Add New
Entry, and then configure the details as shown in the following
figure:
- Type a suitable number in the Stream ID box.
- To enable FMI, select the FMI Enable check box.
- To enable the oversize block, select the Oversize Block Enable checkbox.
- Click Save.
- Click TSN >
PSFP > Flow Meter.
The PSFP Flow Meter Configuration page opens.
Figure 8-5. PSFP Flow Meter Configuration - Click Add New
Entry, and then configure the details as shown in the following
figure:
- To set FMI ID, type a suitable number in the FMI ID box.
- To set CIR (bandwidth in KHz), type a suitable number in the CIR box.
- Click Save.