10.1 Configuring SyncE using Web GUI
To configure SyncE, perform the following steps:
- Click Configuration > SyncE.
- In the Clock Source and
State, ensure the following:
- Check the Nominated Clock source.
- Select the nominated port.
- In the Clock Selection Mode and
State table, ensure the following:
- Make sure the the source is the same as the nominated clock source.
- Set WTR Time to disable.
- In the SyncE Ports table, check the ports that are in use with SyncE.
- Make sure that LOCS, LOL and DHOLD becomes Green.
- Make sure that under the Clock Selection Mode and State section, State becomes Locked.
Note: For a more detailed SyncE configuration guide,
go to SyncE Software Configuration Guide
(microchip.com).