9.5.1 Structure and Union Qualifiers
The MPLAB XC32 C/C++ Compiler supports the use of type qualifiers on structures.
When a qualifier is applied to a structure, all of its members will inherit this
qualification. In the following example the structure is qualified
const.
const struct {
int number;
int *ptr;
} record = { 0x55, &i };
In this case, the entire structure will be placed into the program memory and each member
will be read-only. Remember that all members are usually initialized if a structure is
const as they cannot be initialized at runtime.
If the members of the structure were individually qualified const, but
the structure was not, then the structure would be positioned into RAM, but each member
would be read-only. Compare the following structure with the above.
struct {
const int number;
int * const ptr;
} record = { 0x55, &i};