7.3.1 Syntax
The following shows the meta syntax notation for the different forms the pragma may take.
pragma-config-directive:
# pragma config setting-list
setting-list:
setting
| setting-list, setting
setting:
setting-name = value-name
The setting-name and value-name are device specific and can be determined by using the PIC32ConfigSet.html document located in the installation directory, docs folder.
All #pragma config directives should be placed outside of a function
definition as they do not define executable code.
PIC32MZ config pragmas include config_alt, config_bf1,
config_abf1, config_bf2, and
config_abf2 pragmas to support placing configuration bit values in
the alternate, boot flash 1, alternate boot flash 1, boot flash 2, and alternate boot
flash 2 PIC32MZ memory regions, respectively. (Example: #pragma config_bf2
FWDTEN=off)
Integer values for config pragmas can be set using the config and
config_region pragmas. (Examples: #pragma config_bf2 TSEQ =
1 and #pragma config USERID = 0x1234u)