25.3.15 The Allocation Order of Bit-Field
The memory ordering of bit-fields into their storage unit is not specified by the C Language Standard. In the CCI, the first bit defined is the least significant bit (LSb) of the storage unit in which it is allocated.
Example
struct {
unsigned lo : 1;
unsigned mid :6;
unsigned hi : 1;
} foo;The bit-field lo is assigned the least significant bit of
the storage unit assigned to the structure foo. The bit-field
mid is assigned the next 6 least significant bits, and
hi, the most significant bit of that same storage unit byte.
Differences
This is identical with the previous operation of all compilers.
Migration to the CCI
No action required.