22.3 Pragma Directives
There are certain compile-time directives that can be used to modify the behavior of the
compiler. These are implemented through the use of the ANSI standard
#pragma facility. Any pragma which is not understood by the
compiler will be ignored.
#pragma keyword optionswhere
keyword is one of a set of keywords, some of
which are followed by certain options. A description
of the keywords is given below.#pragma config
The #pragma config directive specifies the
processor-specific configuration settings (that is, Configuration bits) to be used by
the application. See 7.3 Configuration Bit Access.
default_function_attributes
The default_function_attributes = [@ "section"] pragma
sets default section placement attributes for function declarations and definitions that
do not otherwise specify this attribute. All functions after the pragma will be placed
in the section whose name is quoted after the @ token. Using the
default_function_attributes = form of this pragma will reset the
section specification, so that subsequent functions are not placed in any special
section.
default_variable_attributes
The #pragma default_variable_attributes = [@ "section"]
pragma sets default section placement attributes for variable declarations and
definitions that do not otherwise specify this attribute. All variables after the pragma
will be placed in the section whose name is quoted after the @ token.
Using the #pragma default_variable_attributes = form of this pragma
will reset the section specification, so that subsequent variables are not placed in any
special section.
#pragma interrupt
Mark a function as an interrupt handler. The prologue and epilogue code for the function
will perform more extensive context preservation. Note that the
interrupt attribute (rather than this pragma) is the recommended
mechanism for marking a function as an interrupt handler. The interrupt pragma is
provided for compatibility with other compilers. See 17 Interrupts and 17.4 Exception Handlers.
#pragma message
The message = "text" pragma prints the quoted text at
build time, as neither a warning nor error, but purely as an advisory.
#pragma GCC optimize
#pragma GCC optimize ("string"...) pragma sets
default optimization attributes for function declarations and definitions that do not
otherwise specify these attributes. All functions after the pragma will be optimized
accordingly. The parentheses are optional. The arguments allowed may be:- A number
n, to be interpreted as an optimization level, i.e., the-Onoption. - A string beginning with
O, which is interpreted as an optimization option, i.e.,-Ostring. - Otherwise,
stringshould be an option that can be used with a-fprefix.
#pragma GCC reset_options pragma clears the default
optimizations, so that the optimization of subsequent functions is not controlled by
optimize pragma.#pragma pack
The #pragma pack pragma allows the maximum alignment of members of
structures (other than zero-width bit-fields), unions, and classes to be changed. All
aggregate objects after the pragma will be packed accordingly. subsequently defined.
The #pragma pack(n) form of this pragma specifies the
new packing alignment. The n value should be a small
power of two and specifies the new packing alignment in bytes.
The #pragma pack() form of this pragma resets the packing alignment to
that in effect when compilation started. This might have been specified with the
-fpack-struct option.
The #pragma pack(push[,n]) form of this pragma pushes
the current alignment setting on an internal stack and then optionally sets the new
packing alignment to the value n.
The #pragma pack(pop) form of this pragma restores the alignment setting
to the one saved at the top of the internal stack by a previous #pragma
pack(push) (and removes that stack entry).
#pragma vector
Generate a branch instruction at the indicated exception vector that targets the
function. Note that the vector attribute (rather than this pragma) is
the recommended mechanism for generating an exception/interrupt vector. See 17 Interrupts and 17.4 Exception Handlers.
#pragma weak
The #pragma weak pragma can be used to declare weak symbols and defining
weak aliases.
The #pragma weak symbol form of this pragma declares
symbol to be weak, as if the declaration had used the weak attribute.
The pragma can appear before or after the declaration of
symbol, or can be used in situations where symbol
is never defined.
The #pragma weak symbol1 = symbol2
form of this pragma declares symbol1 to be a weak
alias of symbol2. The
symbol2 symbol must be defined in the current
translation unit.