15.3.6 Example Stack Report
For this simple example, assumed to be stored in a file named
test.c,
int max(int a, int b){
if (a < b)
return b;
return a;
}
int main() {
int a[10], i, j;
for (i =0; i < 10; i++)
a[i] = i;
for (i = 0; i < 10; i++)
a[i] = max(a[i], a[10-i/2]);
return a[0];
}when built
with:xc32-gcc -mprocessor=32MZ2048ECH100 -mchp-stack-usage -O0 mips_stack_guidance.cthe
compiler will print the following stack-usage report.============= STACK USAGE GUIDANCE =============
In the call graph beginning at _reset,
104 bytes of stack are required.
However, the following cautions exists:
1. Indeterminate stack adjustment has been detected:
_main_entry uses 104 bytes
__pic32_software_reset uses 24 bytes
No stack usage predictions can be made.
2. The following functions cannot be connected to the main call graph.
This is usually caused by some indirection:
__DbgExecReturn uses 24 bytes
_bev_exception uses 48 bytes
_gen_exception uses 136 bytes
simple_tlb_refill_vector uses 136 bytes
_cache_err_vector uses 136 bytes
__pic32_size_cache uses 0 bytes
_DefaultInterrupt uses 24 bytes
You must add stack allowances for those functions.
================================================