5.7.1.26 Soft-float Option
The -msoft-float option indicates to the compiler that floating-point
calculations in generated code should be emulated rather than performed by the hardware
floating-point unit (FPU). A variant of the library that does not use hardware
floating-point is also selected for link time.
This option does not typically need to be specified, as the compiler will use an appropriate library and generate suitable floating-point code based on information provided by the Device Family Pack associated with the selected device.