15.2.1 Function Attributes
access(access-mode, ref-index[,
size-index])
The access attribute provides additional information about how a function
accesses memory. It can assist in diagnosing potential bugs related to memory access via
compiler warnings and help the compiler perform better optimizations.
The ref_index argument is the index (starting from the left
with index 1) of the function pointer argument that points to the target object being
accessed. A function pointer argument can be referenced by at most one distinct
access attribute.
access_mode argument specifies the type of memory
access made by the pointer referenced by the ref_index and
can be one of:read_only- The pointer only reads from the target object. Unless the indexed size argument is
zero, the target object must be initialized. This check is more robust than just using
the
constqualifier with the target as it cannot be cast away. write_only- The pointer (which cannot be to a
const-qualified type) only writes to the target object. The object referenced by the pointer need not be initialized. read_write- The pointer (which cannot be to a
const-qualified type) both reads from and writes to the target object. Unless the indexed size argument is zero, the target object must be initialized. none- The pointer does not access the target object at all. Unless the pointer is
NULL, the target object must exist and have at least the size held by the size-index argument. If the size-index argument is omitted for a pointer ofvoid *type, the actual pointer argument is ignored. The referenced object need not be initialized. The mode is intended to be used as a means to help validate the expected object size, for example in functions that call__builtin_object_size.
The optional size_index argument is the index of the
function argument that specifies the number of elements of the pointer type referenced by
ref-index, or the number of bytes when the pointer type
is void *. When this argument is not specified, the pointer argument must be
either NULL or point to a space that is suitably aligned and sized for at
least one object of the referenced type (this implies that a past-the-end pointer is not a
valid argument). The actual size of the access may be less but it must not be more.
access attribute to declare that
the pointer argument to puts() will only read its target of unspecified size.
The attribute is used again to indicate that the second argument to memcpy()
only reads its target and that this target has a size indicated by the value of the third
function
argument.__attribute__ ((access (read_only, 1))) int puts(const char *);
__attribute__ ((access (read_only, 2, 3))) void * memcpy(void *, const void *, size_t);address(addr)
The address attribute specifies an absolute physical address at which the attributed routine will be placed in memory. It can be used with C and C++ functions.
address attribute specifies an absolute virtual address for the function. Be
sure to specify the address attribute using an appropriate virtual address
for the target device. The address is typically in the range [0x9D000000,0x9D0FFFFC], as
defined in the linker script as the kseg0_program_mem memory region. For
example:__attribute__((address(0x9D008000))) void bar (void);The compiler performs no error checking on the address. The section containing the function will be located at the specified address regardless of the memory-regions specified in the linker script or the actual memory ranges on the target device. The application code must ensure that the address is valid for the target device.
Sections used to hold functions placed at an absolute address will use a name
.address.N.decl, where
N is the address and
decl is the name of the declaration.
To make effective use of absolute sections and the new best-fit allocator, standard program-memory and data-memory sections should not be mapped in the linker script. The built-in linker script does not map most standard sections such as the .text, .data, .bss, or .ramfunc sections. By not mapping these sections in the linker script, we allow these sections to be allocated using the best-fit allocator rather than the sequential allocator. Sections that are unmapped in the linker script can flow around absolute sections, whereas sections that are linker-script mapped are grouped together and allocated sequentially, potentially causing conflicts with absolute sections.
alias ("symbol")
Indicates that the function is an alias for another symbol. For example:
void foo (void) { /* stuff */ }
__attribute__ ((alias("foo"))) void bar (void);Symbol bar is considered to be an alias for the symbol foo.
always_inline
inline, always inline the function, even if no
optimization level was specified, for
example:void __attribute__ ((always_inline)) foo (void);at_vector
void __attribute__ ((interrupt(IPL4SOFT))) __attribute__ ((at_vector(54)))
foo void);
See also Interrupts and Exception Handlers.
const
const, allowing for even
more aggressive optimization. Note that a function which de-references a pointer argument is
not const since the pointer de-reference uses a value which is not a
parameter, even though the pointer itself is a parameter. For
example:int __attribute((const)) rv(int a);deprecated
deprecated (msg)
deprecated is used, a warning is generated. The
optional msg argument, which must be a string, will be printed in the warning if
present, for
example:void __attribute__ ((deprecated ("The bar function is no longer used"))) bar (void);
The deprecated attribute may also be used for variables and types.externally_visible
-fwhole-program command-line option, so the function remains visible
outside the current compilation unit, for
example:void __attribute__((externally_visible)) foo (void);This
might prevent certain optimizations from being performed on the function.far
CALL instruction. For
example:void __attribute__((far)) foo (void);format (type, format_index, first_to_check)
format attribute indicates that the function takes a
printf, scanf, strftime, or
strfmon style format string and arguments and that the compiler should type
check those arguments against the format string, just as it does for the standard library
functions, for
example:extern int __attribute__ ((format (printf, 2, 3))) my_printf (void *my_object, const char *my_format, ...);
The type parameter is one of printf, scanf, strftime or strfmon (optionally with surrounding double underscores, for example, __printf__) and determines how the format string will be interpreted.
The format_index parameter specifies which function parameter is the format string. Function parameters are numbered from the left-most parameter, starting from 1.
The first_to_check parameter specifies which parameter is the first to check against the format string. If first_to_check is zero, type checking is not performed and the compiler only checks the format string for consistency (for example, vfprintf).
format_arg (index)
format_arg attribute specifies that a function manipulates a
printf style format string and that the compiler should check the format
string for consistency. The function attribute which is a format string is identified by
index. For
example:extern char * __attribute__ ((format_arg (2))) my_foo (char *my_str, const char *my_format);function_replacement_prologue
This feature allows the application to redirect one function to another implementation at runtime without replacing the existing function. This is achieved by changing the method of invoking functions through a function replacement table instead of from a linker-resolved address. Initially the function address in the table points to the location of the entry point of the original function's prologue. The application can then replace the table entry with the new function address. Now, during the program execution, the control will pass to the new function address and returns to the caller function. This feature adds a new function_replacement_prologue function attribute. To redirect the function, modify the corresponding Function Replacement Table entry at runtime.
Example C code:
int a, b, c, d;
int __attribute__((function_replacement_prologue)) foo (void)
{
a = b + c;
return (a);
}
int main()
{
d = foo();
return 0;
}Example generated assembly code:
# Function Replacement Table entries, located in data memory
.section .fixtable, data
fixtable.foo:
.word cont.foo # By default, populate the table with the address
# of the original implementation. Redirect to
# another implementation by overwriting this
# location with the address of the new implementation.
.section .text, code
.globl foo
.ent foo
.type foo, @function
foo:
# Begin Function Replacement Table Prologue
lui $25,%hi(fixtable.foo) # Load address from .fixtable above
lw $25,%lo(fixtable.foo)($25)
j $25 # Jump to address loaded from table
nop
cont.foo:
# End Function Replacement Table Prologue
addiu $sp,$sp,-8
sw $fp,4($sp)
move $fp,$sp
lw $3,%gp_rel(b)($28)
...........
j $31
nopinterrupt (priority)
Generate prologue and epilogue code for the function as an interrupt handler function. See Interrupts . The argument specified the interrupt priority level using the symbols IPLnSOFT, IPLnSRS, or IPLnAUTO where n represents the 7 levels of priority and SOFT|SRS|AUTO specifies the context saving mode.
keep
__attribute__((keep)) may be applied to a function. The keep attribute will
prevent the linker from removing the function with --gc-sections, even if it
is unused, for
example:void __attribute__((keep)) foo(void);longcall
far, for
example:void __attribute__((longcall)) foo (void);malloc
void __attribute__ ((malloc)) *custom_malloc (int size_t); This
allows the compiler to improve optimization.micromips
void __attribute__ ((microcmips)) foo(void);mips16
void __attribute__ ((mips16)) foo(void);naked
void __attribute__ ((naked)) foo(void);near
CALL instruction, even when the
-mlong-calls command line option is specified, for
example:void __attribute__ ((near)) foo(void);no_fpu
no_fpu attribute must be used in conjunction with the interrupt
(priority) attribute and specifies that the interrupt service routine (ISR) should
not preserve the Floating-Point Unit (FPU) context. In addition it causes the compiler to
insert code into the ISR that will disable the FPU, by clearing the CU1 bit of the CP0 Status
register. If your ISR attempts to perform floating-point operations while the FPU is disabled,
the device will trigger a general exception. This also means that any higher-priority ISR
interrupting an ISR using the no_fpu attribute must re-enable the FPU if
floating-point operations are required. The ISR restores the original value of the status
register before returning from the interrupt. For
example:void __attribute__((interrupt(IPL7SRS), vector(_CORE_TIMER_VECTOR), no_fpu)) isr(void);noinline
void __attribute__ ((noinline)) foo(void);noload
noload
attribute set. It tells consumers of the ELF files not to load the contents of the section.
This attribute can be useful when you just want to reserve memory for something, but you don’t
want to clear or initialize memory. For
example:void __attribute__ ((noload)) foo(void);nomips16
-mips16 command line option, for
example:void __attribute__ ((nomips16)) foo(void);nonnull (index, ...)
Indicate to the compiler that one or more pointer arguments to the function must be non-null. If the compiler determines that a Null Pointer is passed as a value to a non-null argument, and the -Wnonnull command line option was specified, a warning diagnostic is issued.
nonnull attribute, all pointer arguments of the
function are marked as non-null. For
example:void * __attribute__((nonnull)) my_memset (void * ptr, int x, size_t len);noreturn
noreturn should always have a return type of void. For
example:void __attribute__ ((noreturn)) myExit(void);optimize(optimization)
optimize attribute allows a function to be built with optimizations that
differ from what has been specified on the command line and which will be applied to the rest
of the program. The optimization argument can either be a
number or a string. String arguments represent the command-line option used to control an
optimization, for example, to enable peephole optimizations (-fpeephole), use
optimize("peephole"). The -f option prefix does not need
to be specified with the argument. If you want to specify more than one optimization, separate
the arguments with commas but with no space characters. Arguments that begin with
O are assumed to be an optimization level option, for example
optimize("O1,unroll-loops") turns on level 1 optimizations and the
unroll-loops optimizations (controlled by the -funroll-loops command-line
option). A numerical argument is also assumed to be an optimization level, for example
optimize(3) turns on level 3 optimizations and is equivalent to the full
usage of the attribute in the following example.
int __attribute__((optimize("O3"))) pandora (void) {
if (maya > axton)
return 1;
return 0;
}This
feature can be used, for instance, to have frequently executed functions compiled with more
aggressive optimization options that produce faster and larger code, while other functions can
be called with less aggressive options. Typically, however, it is not used for production
builds.pure
pure attribute, for
example:void __attribute__ ((pure)) foo(void);ramfunc
The ramfunc attribute locates the attributed routine in RAM rather than in
Flash memory on devices that normally execute code from Flash. This attribute can be used for
both C functions and C++ class methods. The compiler's default runtime startup code uses the
data-initialization template to copy the code associated with functions using this attribute
from Flash to RAM at program startup.
When this attribute is used with C functions, the function is placed at the highest appropriately
aligned address for executable code. Note that due to ramfunc alignment and
placement requirements, the address attribute should not be used with the
ramfunc attribute. The presence of the ramfunc section
causes the linker to emit the symbols necessary for the crt0.S start-up
code to initialize the bus matrix appropriately for executing code out of data memory.
far/longcall attribute and the
section attribute. For
example: __attribute__((ramfunc,section(".ramfunc"),far,unique_section))
unsigned int myramfunct (void_
{ /* code */ }<sys/attribs.h> header file makes the ramfunc
attribute simple to
use: #include <sys/attribs.h>
__longramfunc__ unsigned int myramfunct (void)
{ /* code */ }class printmyname {
// Access specifier
public:
// Data Members
string myname;
int dummy ;
// Member Functions()
printmyname (){
myname = "microchip";
}
void __attribute__((ramfunc, long_call)) set_name(string newname){
myname = newname;
dummy = 9;
}
void printname() { cout << "name is:" << myname; }
};section("name")
Place the function into the named section.
For example:
void __attribute__ ((section (".wilma"))) baz () {return;}
Function baz will be placed in section .wilma.
The -ffunction-sections command line option has no effect on functions defined with a section attribute.
unique_section
Place the function in a uniquely named section, as if -ffunction-sections had been specified. If the function also has a section attribute, use that section name as the prefix for generating the unique section name.
For example:
void __attribute__ ((section (".fred"), unique_section) foo (void) {return;}
Function foo will be placed in section .fred.foo.
unused
void __attribute__ ((unused)) opt_setting(void);used
static function. For
example:void __attribute__ ((used)) foo(void);vector (num)
void __attribute__((vector(0), interrupt(IPL7AUTO))) myisr(void);warn_unused_result
void __attribute__ ((warn_unused_result)) foo(void);weak
void __attribute__ ((weak)) foo(void);