8.11.2 Alias Variable Attribute
The
alias ("symbol") attribute indicates that
the variable is an alias for another symbol. For
example:int var_target;
extern int __attribute__ ((alias ("var_target"))) var_alias;defines
var_alias to be an alias for the
var_target variable.It is an error if the alias target is not defined in the same translation unit as the alias.