8.11.14 Uninitialized Variable Attribute
The uninitialized attribute is used with objects having
automatic storage duration and indicates to the compiler that the object
should not be automatically initialized when the option
-ftrivial-auto-var-init is in effect.
The -ftrivial-auto-var-init option forces
all automatic variables that do not have explicit initializers to be
assigned a value by the compiler. These additional compiler initializations
can incur a significant run-time overhead. Use this attribute to exclude
selected objects from this initialization, in order to reduce runtime
overhead. This attribute has no effect when the
-ftrivial-auto-var-init option has not been
specified.