13.1 Sleep Mode Operation
Sleep mode is entered by executing the SLEEP
instruction.
Upon entering Sleep mode, the following conditions exist:
- Resets other than WDT are not affected by Sleep mode; WDT will be cleared but keeps running if enabled for operation during Sleep.
- The PD bit is cleared.
- The TO bit is set.
- The CPU and the System clocks are disabled.
- LFINTOSC and/or HFINTOSC will remain enabled if any peripheral has requested them as a clock source or if the HFOEN, MFOEN or LFOEN bits are set.
- ADC is unaffected if the ADCRC oscillator is selected. When the
ADC clock is something other than ADCRC, a
SLEEPinstruction causes the present conversion to be aborted and the ADC module is turned off, although the ADON bit remains active. - I/O ports maintain the status they had before
SLEEPwas executed (driving high, low, or high-impedance) only if no peripheral connected to the I/O port is active.
Refer to individual sections for more details on peripheral operation during Sleep.
To minimize current consumption, the following conditions need to be considered:
- I/O pins will not be floating
- External circuitry sinking current from I/O pins
- Internal circuitry sourcing current from I/O pins
- Current draw from pins with internal weak pull-ups
- Modules using any oscillator
I/O pins that are high-impedance inputs need to be pulled to VDD or VSS externally to avoid switching currents caused by floating inputs.