3.1 Single-step Assembly
Assembly of one or more source files can be performed in just one step using the
                pic-as driver.
The following command will build both the assembly source files, passing these files to the appropriate internal applications, then link the generated code to form the final output.
pic-as -mcpu=16F877A main.S mdef.s
        The driver will compile all source files, regardless of whether they have changed since the last build. Development environments (such as MPLAB® X IDE) and make utilities must be employed to achieve incremental builds (see Multi-step Assembly).
Unless otherwise specified, a HEX file and ELF file are produced as the final
            output. The intermediate files remain after compilation has completed, but most other
            temporary files are deleted, unless you use the -save-temps option (see
                Save-temps Option) which
            preserves all generated files. Note that some generated files can be in a different
            directory than your project source files (see also O: Specify Output File).