3.4 Assembler Option Descriptions
Most aspects of the build process can be controlled using options passed
to the assembler's command-line driver, pic-as.
All options are case sensitive and are identified by leading single or
double dash character, e.g. -o or --version.
Use the --help option to obtain a brief description of
accepted options on the command line.
If you are compiling from within the MPLAB X IDE, it will issue explicit options to the assembler that are based on the selections in the project's Project Properties dialog. The default project options might be different to the default options used by the assembler when running on the command line, so you should review your IDE properties to ensue that they are acceptable.
The summary of all available driver options tabulated below is followed by a detailed description of each option.
| Option (Links to explanatory section) | Controls |
|---|---|
-c | Generation of an intermediate object file |
-Dmacro=text | Definition of preprocessor symbols |
-dM | List all defined macros |
-E | The generation of preprocessed-only files |
--fill=options | Filling of unused memory |
-fmax-errors | Number of errors before aborting |
-gformat | The type of debugging information generated |
-H | List included header files |
--help | Display help information only |
-Idir | Directories searched for headers |
-llibrary | Which libraries are scanned |
-Ldir | Directories searched for libraries |
-mcallgraph=type | The type of callgraph printed in the map file |
-mchecksum=specs | The generation and placement of a checksum or hash |
-mcpu=device | The target device that code will be built for |
-mdfp=path | Which device family pack to use |
-m[no-]download | How the final HEX file is conditioned |
-misa=set | Select PIC18 instruction set |
-mmaxichip | Use of a hypothetical device with full memory |
-mprint-devices | Chip information only |
-mram=ranges | Data memory that is available for the program |
-mreserve=ranges | What memory should be reserved |
-mrom=ranges | Program memory that is available for the program |
-mserial=options | The insertion of a serial number in the output |
-msummary=types | What memory summary information is produced |
-mwarn=level | The threshold at which warnings are output |
-o
file | Specify output file name |
-save-temps | Whether intermediate files should be kept after compilation |
-Umacro | The undefining of preprocessor symbols |
-v | Verbose compilation output |
--version | Display of assembler version information |
-w | The suppression of all warning messages |
-Wa,option | Options passed to the assembler |
-W[no-]error | Promote warnings to errors |
-Wp,option | Options passed to the preprocessor |
-Wl,option | Options passed to the linker |
-xlanguage | The language in which the source files are interpreted |
-Xassembler
option | Options passed to the assembler |
-Xpreprocessor
option | Options passed to the preprocessor |
-Xlinker option | System-specific options to passed to the linker |