7.2.3.1 Specifications and Filenames
Hexmate can process Intel HEX files that conform to a variety of formats, as discussed in HEX File Formats. Hex files typically use a .hex extension; however this is not mandatory when using Hexmate.
Additional specifications can be applied to each HEX file listed on the command line to place conditions on how this file should be processed. If any specifications are used, they must precede the name of the file they correspond to, using a comma to separate them from the filename.
rStart-End
, where
Start
and End
are
both assumed to be hexadecimal addresses, whose interpretation is based on the addressing
value (see Addressing Hexmate Option). Hexmate
will only process data within the address range restriction. For example, assuming that the
addressing value is 1, the
specification:r100-1FF,myfile.hex
will tell Hexmate
to use myfile.hex as an input file but that it should only process
data from that file that has HEX file addresses within the range 0x100-1FF (inclusive).sOffset
, where
Offset
is assumed to be an unqualified hexadecimal
value. If an address shift is used, data read from this HEX file will be shifted (by the
offset specified) to a new HEX file address in the output file. The offset can be either
positive or negative. For example, the
specification:r100-1FFs2000,myfile.hex
will shift
the block of data from 0x100-1FF in myfile.hex
to the new HEX file address
range 0x2100-21FF in the output.Be careful when shifting data containing executable code. Program code should only be shifted if it is position independent.