1.4.1.5 Bootloader Verification Method
- Summary
-
Select the method used to verify the application binary
- Description
-
Provides the ability to select between multiple verification methods. An overview of the verification methods is described in Application Verification Overview. If checksum is used, the user can update the default addresses in the bootloader::application configuration in Application Configuration Dialog.