3.2 Foundation Services
To generate this project using Foundation Services (FS), follow the next steps:
- Create a new MPLAB X IDE project for PIC18F47Q10.
- Open MCC from the toolbar (more information on how to install the MCC plug-in can be found in the reference list).
- Go to Project Resources →
System → System Module and do the following configuration:
- Oscillator Select: HFINTOSC
- HF Internal Clock: 64 MHz
- Clock Divider: 1
- In the Watchdog Timer Enable field in the WWDT tab, WDT Disabled has to be selected
- In the Programming tab, Low-Voltage Programming Enable has to be checked
- From the Device Resources window, add
I2CSIMPLE, then do the following configuration:
- Select I2C Host: MSSP1
- Go to Device Resources → Peripherals → MSSP1, then check the Interrupt Driven box.
- Open the Pin Manager → Grid
View window, select UQFN40 in the MCU package field and do
the following pin configurations:
Figure 3-4. Pin Mapping - Go to Project Resources → Pin Module, and set both pins, RB1 and RB2, to use the internal pull-up by checking the box in the WPU column.
- In the Project Resources window, click the Generate button so that MCC will generate all the specified drivers and configurations.
- Edit the
main.cfile, as following:
#include "mcc_generated_files/mcc.h" #define I2C_CLIENT_ADDR 0x20 #define MCP23008_REG_ADDR_IODIR 0x00 #define MCP23008_REG_ADDR_GPIO 0x09 #define PINS_DIGITAL_OUTPUT 0x00 #define MCP23008_DATA 0x0F /* Main application */ void main(void) { // Initialize the device SYSTEM_Initialize(); // Enable the Global Interrupts INTERRUPT_GlobalInterruptEnable(); // Enable the Peripheral Interrupts INTERRUPT_PeripheralInterruptEnable(); /* Set data to use in the I2C operations */ uint8_t data = MCP23008_DATA; /* Set the extended pins as digital output */ i2c_write1ByteRegister(I2C_CLIENT_ADDR, MCP23008_REG_ADDR_IODIR, PINS_DIGITAL_OUTPUT); while (1) { /* Write data to the GPIO port */ i2c_write1ByteRegister(I2C_CLIENT_ADDR, MCP23008_REG_ADDR_GPIO, data); /* Read data from the GPIO port */ data = i2c_read1ByteRegister(I2C_CLIENT_ADDR, MCP23008_REG_ADDR_GPIO); /* Overwrite data with the inverted data read */ data = ~data; __delay_ms(500); } }