3.1 MCC Generated
To generate this project using MPLAB Code Configurator (MCC), follow the next steps:
- Create a new MPLAB X IDE project for PIC18F47Q10.
- Open MCC from the toolbar (more information on how to install the MCC plug-in can be found in the reference list).
- Go to Project Resources → System →
System Module and do the following configuration:
- Oscillator Select: HFINTOSC (default)
- HF Internal Clock: 64 MHz (default)
- Clock Divider: 1
- In the Watchdog Timer Enable field in the WWDT tab, WDT Disabled has to be selected
- In the Programming tab, Low-Voltage Programming Enable has to be checked
- From the Device Resources window, add
Drivers → I2C → I2CSIMPLE, then do the following
configuration:
- I2C_host dependency selector: MSSP1
- Go to Project Resources → Drivers → MSSP
→ MSSP1, then do the following configuration:
- Interrupt Driven: Checked
- Serial Protocol: I2C
- Mode: Host
- I2C Clock Frequency: 100000
- Go to the Pins Grid View, select
UQFN40 in the MCU package field, and do the following pin configurations:
Figure 3-3. Pin Mapping - Go to Project Resources → System → Pin
Module and set both pins, RB1 and RB2, to use the:
- Internal pull-up, by checking the box in the Weak Pullup column
- Open drain, by checking the box in the open drain column
- In the Project Resources window, click the Generate button so that MCC will generate all the specified drivers and configurations.
- Edit the
main.cfile, as following:
#include "mcc_generated_files/system/system.h" #define I2C_CLIENT_ADDR 0x20 #define MCP23008_REG_ADDR_IODIR 0x00 #define MCP23008_REG_ADDR_GPIO 0x09 #define PINS_DIGITAL_OUTPUT 0x00 #define MCP23008_DATA 0xFF /* Main application */ const i2c_host_interface_t *I2C = &i2c1_host_interface; int main(void) { SYSTEM_Initialize(); INTERRUPT_GlobalInterruptEnable(); INTERRUPT_PeripheralInterruptEnable(); uint8_t dataWrite[2]; uint8_t dataRead[1]; dataWrite[0] = MCP23008_REG_ADDR_IODIR; dataWrite[1] = PINS_DIGITAL_OUTPUT; if(I2C->Write(I2C_CLIENT_ADDR, dataWrite,2)) { /* Bus is good */ /* Delay is used as a placeholder for other actions */ __delay_ms(2); } if(!I2C->IsBusy()) { if(I2C1_ErrorGet() == I2C_ERROR_NONE) { /* Transfer is completed successfully */ } else { /* Error occurred during transfer. */ } } dataWrite[0] = MCP23008_REG_ADDR_GPIO; dataWrite[1] = MCP23008_DATA; while(1) { if(I2C->Write(I2C_CLIENT_ADDR, dataWrite,2)) { /* Bus is good */ /* Delay is used as a placeholder for other actions */ __delay_ms(2); } if(!I2C->IsBusy()) { if(I2C1_ErrorGet() == I2C_ERROR_NONE) { /* Transfer is completed successfully */ } else { /* Error occurred during transfer. */ } } if (I2C->Read(I2C_CLIENT_ADDR, dataRead,1)) { /* Bus is good */ /* Delay is used as a placeholder for other actions */ __delay_ms(2); } if(!I2C->IsBusy()) { if(I2C1_ErrorGet() == I2C_ERROR_NONE) { /* Transfer is completed successfully */ } else { /* Error occurred during transfer. */ } } dataWrite[1] = ~dataRead[0]; __delay_ms(1000); } }