3 External Connections
External connections refer to the hardware connections used between the target hardware and the PC. These connections define the type of communication between the target and the MPLAB Data Visualizer. The type of connection depends on the target.
To connect the target to the PC: Follow the instructions for the device or demonstration board.
Once a supported target has been connected to the PC, it should be listed in the Connections tab on the left side. The supported types of communication are:
- DGI Tools - tools or kits that support the Data Gateway Interface. It is capable of input streaming communication over SPI, I2C, USART and Debug GPIO. The feature set varies by tool.
- Serial/CDC Connections - selection specifies communication with any serial port on the system that can be set up using baud rate, parity, data bits and stop bits.
- Curiosity Nano Explorer - supports streaming power data from the embedded Power Monitor.