10.1.4.2 Backup Mode Entry and Wake-Up

The following figure shows the recommended power-down sequence to place the SAM9X7 Series device in Backup mode. The SHDN signal, output of Shutdown Controller (SHDWC), signals the shutdown request to the external power supply. This output is supplied by VDDBU that is present in Backup mode. In a similar way to the power-down sequence, the NRST signal must be asserted prior to turning the SAM9X7 Series power supplies off.

Figure 10-4. Recommended Power Sequence at Backup Mode Entry
Table 10-13. Backup Mode Entry Timing Requirements
SymbolParametersConditionsMinMaxUnit
tSHDNSHDN delay at Backup mode entryDelay from SHDN low to NRST low0ms
tRSTPDNRST delay at power-downDelay from NRST low to the first supply out of its operating range0ms

The following figure shows the recommended power-up sequence to wake up the SAM9X7 series device from Backup mode. Upon a wake-up event (WKUP pin, RTC alarm, etc.), the Shutdown Controller automatically toggles its SHDN output back to VDDBU to request the external power supply to restart. This power-up sequence is the same as the one shown in Figure 10-2. In particular, the supply groups definition is the same.

Figure 10-5. Recommended Power Sequence at Wake-Up from Backup Mode
Table 10-14. Wake-Up from Backup Mode Timing Requirements(1)
SymbolParametersConditionsMinMaxUnit
t0VDDIN33 delayDelay from SHDN high to VDDIN33 turn-on0ms
t1VDDIN33 to periphery group delayDelay from established VDDIN33 to the first established periphery group supply-0.1ms
t2Periphery group to VDDCORE delayDelay from the last established periphery group supply to VDDCORE supply turn-on0ms
t3Reset delay at power-upFrom established VDDCORE to NRST high8ms
Note:
  1. The term "established" refers to a power supply established to 90% of its final value.