18.6.2.3 Reset Causes and Effects

The latest Reset cause is available in RCAUSE register, and can be read during the application boot sequence in order to determine proper action.

These are the groups of Reset sources:

  • Power supply Reset: Resets caused by an electrical issue. It covers POR and BODs Resets
  • User Reset: Resets caused by the application. It covers external Resets, system Reset requests and watchdog Resets
  • Backup reset: Resets caused by a Backup Mode exit condition

The following table lists the parts of the device that are reset, depending on the Reset type.

Table 18-1. Effects of the Different Reset Causes
Power Supply ResetUser ResetBackup Reset
POR, BOD33BOD12External ResetWDT Reset, System Reset RequestRTC, BBPS
RTC, OSC32KCTRL, RSTC, CTRLA.IORET bit of PMYNNNN
GCLK with WRTLOCKYYNNY
Debug logicYYYNY
OthersYYYYY

The external Reset is generated when pulling the RESET pin low.

The POR, BOD12, and BOD33 Reset sources are generated by their corresponding module in the Supply Controller Interface (SUPC).

The WDT Reset is generated by the Watchdog Timer.

The System Reset Request is a Reset generated by the CPU when asserting the SYSRESETREQ bit located in the Reset Control register of the CPU (for details refer to the ARM® Cortex™ Technical Reference Manual on http://www.arm.com).

From Backup Mode, the chip can be waken-up upon these conditions:

  • Battery Backup Power Switch (BBPS): generated by the SUPC controller when the 3.3V VDDIO is restored.
  • Real-Time Counter interrupt. For details refer to the applicable INTFLAG in the RTC for details.

If one of these conditions is triggered in Backup Mode, the RCAUSE.BACKUP bit is set and the Backup Exit Register (BKUPEXIT) is updated.