14.3 Enhanced Configuration with Manual Input of Parameters Example
Below is an enhanced configuration example using the MPLAB Data Visualizer terminal. In this example, the parameters are configured in the following way:
- Operation Mode: Capacitive (option
0) - Sleep time: Four seconds (option
3) - Extended output mode: Serial data enabled (option
1) - Extended output format: Standard
measurement only (option
1) - Confirm the reference value provided (option
0) - Provide the threshold value:
2000