36.9.1 Data Bus Width
A data bus width of 8 or 16 bits can be selected for each chip select. This option is controlled by the bit DBW in the Mode register (HSMC_MODE) for the corresponding chip select.
Figure 36-4 shows how to connect a 512 KB x 8-bit memory on NCS, Figure 36-5 shows how to connect a 512 KB x 16-bit memory on NCS.
Note: NCS represents one of the NCS[0:3] chip select lines. Ax represents A[25].
Note: NCS represents one of the NCS[0:3] chip select lines. Ax represents A[25].