1.22 TC Compare Mode

This example shows how to use the TC module in compare mode to generate an active low, active high, and toggle output on compare match.

Description

Three TC channels are configured in compare mode. Each channel generates different output waveform depending upon configured action on compare match and period match.

Active low output: Output is set high on compare 1 match and is set low on compare 0 match.

Active high output: Output is set low on compare 1 match and is set high on compare 0 match.

Toggle output: Output toggles on compare 0 match.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/tc/tc_compare_mode.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
wbz653_curiosity.XMPLABX Project for WBZ653 Curiosity Board

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
wbz653_curiosity.XWBZ653 Curiosity Board

Setting Up WBZ653 Curiosity Board

  • Connect the Debug USB port on the board to the computer using a micro USB cable.

Running the Application

  1. Build and Program the application using its IDE.
  2. Observe generated waveforms on the oscilloscope.
Timer ChannelPinObservable Characteristic of the Waveform
TC0_WO1PA02 (RX Pin of mikroBUS 1)Active low output with 100 Hz frequency
TC2_WO1PB10 (AN Pin of mikroBUS 1)Active high output with 100 Hz frequency
TC1_WO0PA03 (Pin 25 of GPIO Header)Toggle output with 50 Hz frequency