1.20 Systick Periodic Interrupt

This example shows how to use the SysTick to generate periodic interrupts.

Description

This example application configures the SysTick Peripheral Library to generate periodic ticks. The application registers a periodic timeout callback. It toggles an LED every time the callback is triggered.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/systick/systick_periodic_timeout.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
wbz653_curiosity.XMPLABX Project for WBZ653 Curiosity Board

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
wbz653_curiosity.XWBZ653 Curiosity Board

Setting Up WBZ653 Curiosity Board

  • Connect the Debug USB port on the board to the computer using a micro USB cable.

Running the Application

  • Build and Program the application using its IDE.
  • The LED blinks continuously.

Refer to the table below for details of LED:

BoardLED Name
WBZ653 Curiosity BoardRed LED