3.2 Getting Started with MCHPRT3 RNBD GUI

To run an RF test on the RNBD Family Add-on Board, perform the following procedure:

  1. Connect the Type-C in the Curiosity Board to the PC.
  2. Check whether the jumper for the current measurement was inserted or not.
  3. Run MCHPRT3.exe.
  4. From the “Select GUI” drop-down list, select RNBD.
  5. Click Open to launch the RNBD window.
  6. Select the respective “COM PORT” (check device manager in PC). A different USB-to-UART serial converter requires the corresponding driver; install accordingly.
  7. Baud Rate - 115200 (default value).
  8. Click Connect.
  9. The device is ready for RF test.