3.2.5.1.2 Command Response Pair Example
The following figure shows an example of a host sending the GetClientInfo command to a client and the client responding with an example set of the mandatory parameters.

| Figure Notes | |
| Note 1: | This example contains version 1.0.0 of the MDFU Protocol for the Protocol Version Parameter. When implementing a different version of the protocol, this version must be updated to be the version of the protocol being implemented. |