22.2.1 Capture Sources
In Capture mode, the CCPx pin may be configured as an input by setting the associated TRIS control bit.
Important: If the CCPx pin is configured as an output, a
write to the port can cause a Capture condition.
The capture source is selected by configuring the CTS bits as shown in the following table:
| CTS | Source |
|---|---|
101-111 | Reserved |
100 | IOC Interrupt |
011 | CMP3_output |
010 | CMP2_output |
001 | CMP1_output |
000 | Pin selected by CCPxPPS |