To create a new project, open MPLAB® X
IDE and click on File>New ProjectFigure 3-6. New
Project
In the New Project
pop-up, click on Microchip Embedded>Application
Project(s)>NextFigure 3-7. Choose
Project
In Select Device
window, select the device WBZ451H and click Next.Figure 3-8. Select
Device
In Select Compiler
window, Select the latest compiler and click Next.Figure 3-9. Select
Compiler
In Select Project Name
and Folder window, enter the project name and select the
project location, and click Finish.Figure 3-10. Select
Project Name and Folder
Now MPLAB X Code
Configurator Content Manager will be launched automatically.
Click on
Finish
The MCC
content manager will start downloading the
repositories.Figure 3-11. Downloaded Repositories