1 Harmony 3 Driver and System Service Application Examples for SAM G55 Family
The following applications are provided to demonstrate the typical or interesting usage
models of one or more drivers and system services.
| Name | Description |
|---|---|
| EEPROM Emulator Library Read Write | This application example demonstrates how to read and write to the Emulated EEPROM memory space using the EEPROM Emulator library |
| FAT Filesystem using NVM Media | This application shows an example of implementing a FAT disk in the device internal Flash memory |
| FAT Filesystem using SDSPI Driver and SPI PLIB | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB |
| FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven |
| I2C Driver Asynchronous - I2C EEPROM | This example application demonstrates how to use the I2C driver in asynchronous mode to perform read/write operations on an EEPROM |
| I2C Driver Asynchronous - I2C Multi client | This example application demonstrates the multi-client feature of the asynchronous mode of the I2C driver by communicating with an external EEPROM and a temperature sensor |
| I2C Driver Synchronous - I2C EEPROM | This example application demonstrates how to use the I2C driver in synchronous mode to perform read/write operations on an EEPROM |
| I2C Driver Synchronous - I2C Multi Client | This example application demonstrates the multi-client feature of the synchronous mode of the I2C driver by communicating with an external EEPROM and a temperature sensor |
| I2C EEPROM Driver - AT24 EEPROM Read Write | This example application demonstrates how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM |
| SPI Driver Asynchronous - SPI Multi Client | This example application demonstrates the multi client feature of the asynchronous mode of the SPI driver by reading and writing to two EEPROMs connected to the same SPI bus |
| SPI Driver Synchronous - SPI Multi Client | This example application demonstrates the multi client feature of the synchronous mode of the SPI driver by reading and writing to two EEPROMs connected to the same SPI bus |
| SPI EEPROM Driver - AT25 EEPROM Read Write | This example application demonstrates how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM |
| Time System Service Multi Client | This example application demonstrates the multi-client system timer functionality |
| USART Driver Asynchronous - USART Echo | This example application demonstrates the asynchronous mode of the USART driver by echoing the received characters |
| USART Driver Synchronous - USART Echo | This example application demonstrates the synchronous mode of the USART driver by echoing the received characters |