36.3.7 Bus Time-out
The SMBus protocol requires a bus watchdog to prevent a stalled device from holding the bus indefinitely. The I2C Bus Time-Out (I2CxBTO) register provides several timer sources that can be configured as the time-out time base. When the selected resource expires, the module is reset and the bus is forced into an Idle state.
For example, Timer2 can be selected as the bus time-out source and set to begin counting when the SCL line is low. If Timer2 rolls over before the SCL line transitions high, the module is reset.
1), the module is immediately reset, the SMA and Client Clock
Stretching (CSTR) bits are
cleared, and the Bus Time-out Interrupt Flag (BTOIF) bit is set. If the module is configured in Host mode and the bus time-out event occurs while the host
is active (Host mode Active (MMA) =
1), the module will immediately attempt to transmit a Stop
condition and set the BTOIF bit. Stop condition generation may be delayed if a client
device is stretching the clock but will resume once the clock is released or if the
client holding the bus also times out. The MMA bit is only cleared after the Stop
condition has been generated.
The figure below shows an example of a bus time-out event when the module is operating in Host mode.