15.3.4 NVMREG Write to Program Memory
- Load the address of the row to be programmed into NVMADRH:NVMADRL.
- Load each write latch with data via the NMVDATH:NVMDATL registers.
- Initiate a programming operation.
- Repeat steps 1 through 3 until all data is written.
Before writing to program memory, the word(s) to be written must be erased or previously unwritten. Program memory can only be erased one row at a time. No automatic erase occurs upon the initiation of the write.
Program memory can be written one or more words at a time. The maximum number of words written at one time is equal to the number of write latches. See Figure 15-4 for more details.
The write latches are aligned to the Flash row address boundary defined by the upper ten bits of NVMADRH:NVMADRL, (NVMADRH[6:0]:NVMADRL[7:5]) with the lower five bits of NVMADRL, (NVMADRL[4:0]) determining the write latch being loaded. Write operations do not cross these boundaries. At the completion of a program memory write operation, the data in the write latches is reset to contain 0x3FFF.
1. When the last word to be loaded into the write
latch is ready, the LWLO bit is cleared and the unlock sequence executed. This initiates
the programming operation, writing all the latches into Flash program memory.- Set the WREN bit.
- Clear the NVMREGS bit.
- Set the LWLO bit. When the LWLO bit is set (LWLO =
1), the write sequence will only load the write latches and will not initiate the write to Program Flash Memory. - Load the NVMADRH:NVMADRL register pair with the address of the location to be written.
- Load the NVMDATH:NVMDATL register pair with the program memory data to be written.
- Execute the unlock sequence. The write latch is now loaded.
- Increment the NVMADRH:NVMADRL register pair to point to the next location.
- Repeat steps 5 through 7 until all but the last write latch has been loaded.
- Clear the LWLO bit. When the LWLO
bit is clear (LWLO =
0), the write sequence will initiate the write to Program Flash Memory. - Load the NVMDATH:NVMDATL register pair with the program memory data to be written.
- Execute the unlock sequence. The entire program memory latch content is now written to Flash program memory.
An example of the complete write sequence is shown in Writing to Program Flash Memory. The initial address is loaded into the NVMADRH:NVMADRL register pair; the data is loaded using indirect addressing.
- See Figure 15-2.
Writing to Program Flash Memory
; This write routine assumes the following:
; 1. 64 bytes of data are loaded, starting at the address in DATA_ADDR
; 2. Each word of data is made up of two adjacent bytes in DATA_ADDR,
; stored in little endian format
; 3. A valid starting address (LSb’s = 00000) is loaded in ADDRH:ADDRL
; 4. ADDRH and ADDRL are located in common RAM (locations 0x70 - 0x7F)
; 5. NVM interrupts are not taken into account
BANKSEL NVMADRH
MOVF ADDRH,W
MOVWF NVMADRH ; Load initial address
MOVF ADDRL,W
MOVWF NVMADRL
MOVLW LOW DATA_ADDR ; Load initial data address
MOVWF FSR0L
MOVLW HIGH DATA_ADDR
MOVWF FSR0H
BCF NVMCON1,NVMREGS ; Set Program Flash Memory as write location
BSF NVMCON1,WREN ; Enable writes
BSF NVMCON1,LWLO ; Load only write latches
LOOP
MOVIW FSR0++
MOVWF NVMDATL ; Load first data byte
MOVIW FSR0++
MOVWF NVMDATH ; Load second data byte
MOVF NVMADRL,W
XORLW 0x1F ; Check if lower bits of address are 00000
ANDLW 0x1F ; and if on last of 32 addresses
BTFSC STATUS,Z ; Last of 32 words?
GOTO START_WRITE ; If so, go write latches into memory
CALL UNLOCK_SEQ ; If not, go load latch
INCF NVMADRL,F ; Increment address
GOTO LOOP
START_WRITE
BCF NVMCON1,LWLO ; Latch writes complete, now write memory
CALL UNLOCK_SEQ ; Perform required unlock sequence
BCF NVMCON1,WREN ; Disable writes
UNLOCK_SEQ
MOVLW 55h
BCF INTCON,GIE ; Disable interrupts
MOVWF NVMCON2 ; Begin unlock sequence
MOVLW AAh
MOVWF NVMCON2
BSF NVMCON1,WR
BSF INTCON,GIE ; Unlock sequence complete, re-enable interrupts
return