23.9 Setup for PWM Operation using PWMx Output Pins
The following steps should be taken when configuring the module for PWM operation using the PWMx pins:
- Disable the PWMx pin output driver(s) by setting the associated TRIS bit(s).
- Clear the PWMxCON register.
- Load the T2PR register with the PWM period value.
- Load the PWMxDCH register and bits [7:6] of the PWMxDCL register with the PWM duty cycle value.
- Configure and start Timer2:
- Clear the TMR2IF Interrupt Flag bit of the PIRx register.(1)
- Select the timer clock source to be as FOSC/4 using the T2CLKCON register. This is required for correct operation of the PWM module.
- Configure the CKPS bits of the T2CON register with the Timer2 prescale value.
- Enable Timer2 by setting the ON bit of the T2CON register.
- Enable PWM output pin and wait until Timer2 overflows, TMR2IF bit of the PIRx register is set.(2)
- Enable the PWMx pin output driver(s) by clearing the associated TRIS bit(s) and setting the desired pin PPS control bits.
- Configure the PWM module by loading the PWMxCON register with the appropriate values.
Note:
- In order to send a complete duty cycle and period on the first PWM output, the above steps must be followed in the order given. If it is not critical to start with a complete PWM signal, then move Step 8 to replace Step 4.
- For operation with other peripherals only, disable PWMx pin outputs.