5.1.1.4 BLE Connection
This section explains how to enable scan and connect functionality on the BLE Central Device (PIC32-BZ6). To establish a successful BLE connection, the Advertiser is required to broadcast advertisement packets across the three primary advertisement channels (or a subset of these channels). This allows the devices scanning for advertisers to find and read their advertisement data, the scanner can initiate a connection if advertiser allows it.
- Advertiser (Transmitting Connectable Adv)
- Scanner
Users can choose to either run the precompiled Application Example hex file provided on the PIC32-BZ6 Curiosity Board or follow the steps to develop the application from scratch.
It is recommended to follow the examples in sequence to understand the basic concepts before progressing to the advanced topics.
Recommended Readings
-
Getting Started with Application Building Blocks – See Building Block Examples from Related Links.
-
Getting Started with Peripheral Building Blocks – See Central Devices from Related Links.
-
FreeRTOS and BLE Stack Setup – See Central - FreeRTOS BLE Stack and App Initialize from Related Links.
- See BLE Legacy Scan from Related Links.
- See BLE Connection from Related Links.
- See BLE Transparent UART from Related Links.
-
BLE Software Specification – See MPLAB® Harmony Wireless BLE in Reference Documentation from Related Links.
Hardware Requirement
S. No. | Tool | Quantity |
---|---|---|
1 | PIC32-BZ6 Curiosity Board | 2 |
2 | Micro USB cable | 2 |
SDK Setup
Refer to Getting Started with Software Development from Related Links.
Software Requirement
To install Tera Term tool, refer to the Tera Term web page in Reference Documentation from Related Links.
Smartphone App
None
Programming the Precompiled Hex File or Application Example
Using MPLAB® X IPE:
- Central Device – Import and program the
precompiled hex file:
<Harmony Content Path>\wireless_apps_pic32_bz6\apps\ble\building_blocks\central\central_conn\precompiled_hex
- Peripheral Device – Import and program
the precompiled hex file:
<Harmony Content Path>\wireless_apps_pic32_bz6\apps\ble\building_blocks\Peripheral\Peripheral_conn\precompiled_hex
- For detailed steps, refer to
Programming a Device in MPLAB® IPE in Reference
Documentation from Related Links.Note: Ensure to choose the correct Device and Tool information.
Using MPLAB® X IDE:
- Perform the following the steps mentioned in Running a Precompiled Example. For more information, refer to Running a Precompiled Application Example from Related Links.
- Central Device – Open and program the
application
central_conn.X
located in<Harmony Content Path>\wireless_apps_pic32_bz6\apps\ble\building_blocks\central\central_conn\firmware
. - Peripheral Device – Open and program the
application
peripheral_conn.X
located in<Harmony Content Path>\wireless_apps_pic32_bz6\apps\ble\building_blocks\peripheral\peripheral_conn\firmware
. -
For more details on how to find the Harmony Content Path, refer to Installing the MCC Plugin from Related Links.
Demo Description
To experience this demo, users are required to use “central_connection” and “peripheral_connection” application examples. The two application example mentioned above will demonstrate a BLE Connection Establishment process. An Advertiser (Peripheral) will start connectable, scannable, undirected BLE advertisement and the scanner (Central) will receive the advertisements and initiate a BLE connection. enables users to transmit Connectable and Scannable Undirected BLE Advertisements. Demo application prints the status messages “Scanning” at the initiation of the scan process, “Connected!” upon successful connection, and “Disconnected” when the connection is lost, within a terminal emulator interface.
- Baud Rate/Speed – 115200 (as configured in SERCOM configuration)
- Parity – None
- Data Bits – 8
- Stop Bits – 1
- Flow Control – None
Testing
Users must use another PIC32-BZ6 Curiosity Board configured as peripheral connection, see BLE Connection from Related Links.
This section assumes that a user has already programmed the
peripheral_conn
and central_conn
application on two PIC32-BZ6 Curiosity boards.
- Board 1 – PIC32-BZ6 Curiosity Board Programmed with “peripheral_conn”
- Open TeraTerm and configure as
mentioned below:Terminal Settings:
- Baud Rate/Speed – 115200 (as configured in SERCOM configuration)
- Parity – None
- Data Bits – 8
- Stop Bits – 1
- Flow Control – None
- Reset the board, Upon reset, “Advertising” message is displayed on the TeraTerm.
- Open TeraTerm and configure as
mentioned below:
- Board 2 – PIC32-BZ6 Curiosity Board Programmed with
central_conn
.- Open TeraTerm and configure as
mentioned below:Terminal Settings:
- Baud Rate/Speed – 115200 (as configured in SERCOM configuration)
- Parity – None
- Data Bits – 8
- Stop Bits – 1
- Flow Control – None
- Reset the board. Upon reset, “Scanning” message is displayed on the TeraTerm.
- Upon finding peripheral device with public address {0xA1, 0xA2, 0xA3, 0xA4, 0xA5, 0xA6} message “Found Peer Node” will be displayed and a connection request will be initiated “Initiating connection”.
- Open TeraTerm and configure as
mentioned below:
After connection establishment, both the peripheral device (Board1) and central device (Board2) will display “Connected!” message on respective terminal windows

Developing the Application from Scratch using MCC
- Create a new harmony project. For more details, see Creating a New MCC Harmony Project from Related Links.
- Import component configuration -- This
step helps users setup the basic components and configuration required to develop this
application. The imported file is of format
.mc3
and is located in the path<Harmony Content Path>\wireless_apps_pic32_bz6\apps\ble\building_blocks\central\central_conn\firmware\central_conn.X.
Note: Import and export functionality of Harmony component configuration will help users to start from a known working setup of MCC configuration - Accept dependencies or satisfiers when prompted.
- Verify if the project graph window has
all the expected configuration.
Figure 5-29. Project Graph
Verifying Scan and Connection Configuration
-
Select BLE Stack component in project graph, to open component configuration and configure as illustrated in the following figure.
Figure 5-30. BLE Stack Configuration
Generating a Code
For more details on code generation, refer to MPLAB Code Configurator (MCC) Code Generation from Related Links.
Files and Routines Automatically generated by the MCC
initialization.c
app_ble.c
Source Files | Usage |
---|---|
app.c | Application State machine, includes calls for Initialization of all BLE stack (GAP,GATT, SMP, L2CAP) related component configurations |
app_ble\app_ble.c | Source code for the BLE stack related component configurations, code related to
function calls from app.c |
app_ble\app_ble_handler.c | GAP, GATT, SMP and L2CAP event handlers |
Note:app.c
is autogenerated and has a state machine based Application code sample. Users can use this template to develop their application.
Header Files
ble_gap.h
: This header file contains BLE GAP functions and is automatically included in theapp.c
file
Function Calls
MCC generates and adds the code to initialize the BLE Stack GAP, GATT, L2CAP and SMP in APP_BleStackInit() function
-
APP_BleStackInit()
is the API that will be called inside the Applications Initial State --APP_STATE_INIT
inapp.c
\
User Application Development
Include
- Include the user action. For more information, refer to User Action from Related Links.
-
definitions.h
in all the files where UART will be used to print debug information
Note:definitions.h
is not specific to just UART peripheral, instead it must be included in all application source files where peripheral functionality will be exercised
Start Scanning
// Scanning Enabled
BLE_GAP_SetScanningEnable(true, BLE_GAP_SCAN_FD_ENABLE, BLE_GAP_SCAN_MODE_OBSERVER, 1000);
// Output the state string to UART
SERCOM0_USART_Write((uint8_t *)"Scanning \r\n", 11);
APP_STATE_INIT
in
app.c
. Scan duration is 100 secs. app.c
Scan Results and initiating a BLE connection
-
BLE_GAP_EVT_ADV_REPORT
event inapp_ble_handler.c
is generated upon finding advertisements on legacy channels -
BLE connection can be initiated by using the API
BLE_GAP_CreateConnection(&createConnParam_t);
// code snippet to filter scan results and initiate connection
if ((p_event->eventField.evtAdvReport.addr.addr[0] == 0xA1 && p_event->eventField.evtAdvReport.addr.addr[1] == 0xA2) ||
(p_event->eventField.evtAdvReport.addr.addr[0] == 0xB1 && p_event->eventField.evtAdvReport.addr.addr[1] == 0xB2) ||
(p_event->eventField.evtAdvReport.addr.addr[0] == 0xC1 && p_event->eventField.evtAdvReport.addr.addr[1] == 0xC2))
{
SERCOM0_USART_Write((uint8_t *)"Found Peer Node\r\n", 17);
BLE_GAP_CreateConnParams_T createConnParam_t;
createConnParam_t.scanInterval = 0x3C; // 37.5 ms
createConnParam_t.scanWindow = 0x1E; // 18.75 ms
createConnParam_t.filterPolicy = BLE_GAP_SCAN_FP_ACCEPT_ALL;
createConnParam_t.peerAddr.addrType = p_event->eventField.evtAdvReport.addr.addrType;
memcpy(createConnParam_t.peerAddr.addr, p_event->eventField.evtAdvReport.addr.addr, GAP_MAX_BD_ADDRESS_LEN);
createConnParam_t.connParams.intervalMin = 0x10; // 20ms
createConnParam_t.connParams.intervalMax = 0x10; // 20ms
createConnParam_t.connParams.latency = 0;
createConnParam_t.connParams.supervisionTimeout = 0x48; // 720ms
SERCOM0_USART_Write((uint8_t *)"Initiating Connection\r\n", 23);
BLE_GAP_CreateConnection(&createConnParam_t);
}
app_ble_handler.c
Connected and Disconnected Events
-
All the possible GAP, GATT, SMP and L2CAP Event handlers are available in file
app_ble_handler.c
, users can implement application code to denote connection state here.BLE_GAP_EVT_CONNECTED
event is generated after a successful BLE connection with peripheral device// Connected EVT SERCOM0_USART_Write((uint8_t *)"Connected\r\n", 11); //Disconnected EVT SERCOM0_USART_Write((uint8_t *)"Disconnected\r\n", 15);
Figure 5-36. app_ble_handler.c
Scan Timeout Event
-
In
app_ble_handler.c
BLE_GAP_EVT_SCAN_TIMEOUT
event is generated when BLE Scan duration expires.SERCOM0_USART_Write((uint8_t *)"Scan Completed\r\n", 17);
Figure 5-37. app_ble_handler.c
Where to go from Here
See BLE Transparent UART from Related Links.