5.3.1.1 Expanding/Customising the Application

Configuration for OTA DFU

The MCC project graph for BLE sensor can be seen as below.
The following steps provide the configuration settings for various components which have to be configured as shown.
  1. Enable “DFU module” in “BLE Stack” configuration.
  2. Configuration options for “Over-The- Air Profile” is shown below.
  3. Figure 5-160. PDS_SubSystem configuration
  4. Figure 5-161. System configuration
  5. Figure 5-162. RTOS configuration
  6. Project properties configuration
    Figure 5-163. Header Configuration
    Figure 5-164. OTA Configuration

    After the configurations, click Create OTA File. The Upgradable .bin image with selected “Output File Name” will be created in .X folder. This is the image stored in OTAU Manager to send to OTAU Target.

The BLE Sensor demo protocol based on TRPS profile is a transparent request, response based and not tied only to this BLE sensor application. It can be expanded and customized as per the users need.
  • The protocol parser is implemented in app_trps.c and app_trps.h
    • Request and Response: when user wants to get and modify data on the device
    • Notify: when there is a new data to be sent to mobile app.
  • The protocol commands are defined in app_ble_sensor.h and related sensor functionalities are implemented in app_ble_sensor.c
    • Request and Response: When a command request is received from mobile app, app_trps.c parse the data and forward to specific command callback handler in app_ble_sensor.c
    • Notify: When specific Sensor data to be sent to mobile app, app_ble_sensor.c places the data in data base and calls for notify handler in app_trps.c (/ref APP_TRPS_SendNotification())

Example: To add a command to get temperature in Fahrenheit

Complete the SDK Setup and open the “ble_sensor.x” located in <Discover Path>\wireless_apps_pic32_bz6\apps\ble\advanced_applications\ble_sensor\firmware using MPLABX IDE Changes to - app_ble_sensor.h
  1. Define request, response, size of response payload (not including size of length byte and response ID)
  2. Define a new control command ID
  3. Define a new control command response
  4. Define the length for the new response command
  5. Inside the existing APP_TRPS_SensorData_T structure, add the new data structure which holds the response data
  6. Increase the list size BLE_SENSOR_CMD_RESP_LST_SIZE by one
  7. Add new command request/response set in BLE_SENSOR_DEFINE_CTRL_CMD_RESP() list
Changes to - app_ble_sensor.c
  1. Read the temperature periodically and store in above defined data structure. Add the below code in App_TRPS_Sensor_TimerHandler()
  2. After doing the above changes follow the instruction in select option Build Project in IDE to compile the application example
  3. Select option Run Project in IDE to program the target – the onboard debugger will program the example application

Testing with MBD mobile app

The “BLE Sensor” sub app in MBD mobile app is designed only to work with specific functionality. So, if new command is added in BLE sensor application, “BLE Sensor” mobile app will not know about it. To test the above newly added code, “BLE Smart” sub app in MBD can be used. Follow the below screenshots after launching MBD mobile app.
Note: The command “0x8A 02 10 01” is used to turn the LED on. The control request ID for the on request is the “0x10” within the command. See the tables in section “BLE Sensor Application Control and Sensor Command/Response” below for more details on the commands.
Note: The response “0x8A 03 41 01 00” is notifying the temperature in Celsius (0x100 => 25.6℃). The control response ID for the temperature data is the “0x41” within the command. See the tables in section “BLE Sensor Application Control and Sensor Command/Response” below for more details on the responses.