5.3.1.3 Protocol Exchange

The communication protocol exchange between mobile app (BLE central) and PIC32WM-BZ6204UE module (BLE peripheral) is explained here.

1. BLE Sensor Data in Advertising Beacon:

  • Advertisement Data:

    • Service UUID: 16-bit Service UUID, 0xFEDA is purchased by Microchip from Bluetooth SIG.

    • BLE Sensor data: 0x40+Light ON/Off status (1 Byte)+ 0x41+Temperature data (2 bytes)

  • Scan Response Data:

    • The device name is part of the scan response. Device name is set as "BLE_SENSOR_XXXX” (XXXX means the last two bytes of the device address).

2. Transparent Profile and Service (TRP/TRS):

Transparent Profile and Service (TRP/TRS) is the proprietary BLE service by microchip to establish data and control channel between BLE Central (Phone) and Peripheral (device).

  • Transparent Profile (TRP) enables higher layer application to control and allow data exchange between TRP Client and Server devices

  • Transparent Service (TRS) includes both Ctrl and Data Pipes which are custom 128-bit GATT characteristics.

    • The Transparent Server shall be a GATT Server

    • The Transparent Client shall be a GATT Client

      Definition of Transparent Service and Characteristics UUID's

      Characteristic NameUUIDProperties
      TRS Service49535343-FE7D-4AE5-8FA9-9FAFD205E455
      TRS TxD- Tx Data to Client role (Data pipe)49535343-1E4D-4BD9-BA61-23C647249616Notify, Write
      TRS TxD - Client Characteristic Configuration DescriptorRead, Write
      TRS RxD- Rx Data from Client role (Data pipe)49535343-8841-43F4-A8D4-ECBE34729BB3Write, Write without response
      TRS Ctrl Pt - Command and Response (Ctrl pipe)49535343-4C8A-39B3-2F49-511CFF073B7ENotify, Write, Write without response
      TRS Ctrl Pt - Client Characteristic Configuration descriptorRead, Write

3. BLE Sensor Application over Transparent Service Control Point (TRS Ctrl Pt):

BLE Sensor application uses TRS Control Point Characteristic of TRPS profile to exchange data between mobile phone and device.

The BLE Sensor application follows the following protocol format on TRS control point characteristic.

ItemOpcodeLengthSensor/Control IDPayload
Size1 Byte1 Byte1 ByteVariable

The description of each element is as below:

- The Opcode: (0x8A) is fixed 1 byte in size and related to BLE Sensor/Control commands.
- Length: 1 byte in size (size of Sensor/Control ID + size of Payload)
- The Sensor/Control ID: 1 byte in size. It could be divided into Control request, Control response, Sensor notify data described in detail in following sections.
- The Sensor/control data and payload size depends on the Sensor/Control ID as listed in the below table.

BLE Sensor Application Control and Sensor Command/Response

Control CmdOpcodeControl Request IDParameterParameter Length (Byte)Control Response IDControl Response PayloadControl Response Payload Length (Byte)Description
RGB LED On/Off Set0x8A0x10On/Off10x20Status code1Switch On/Off the RGB LED with the default/last set color
RGB LED On/Off Get0x8A0x110x21Status code + On/Off status2Send the RGB LED on/off status
RGB Color Set0x8A0x12Color value (HSV)30x22Status code1Set RGB color value in HSV format
RGB Color Get0x8A0x130x23Status code + RGB color value4Send RGB color value in HSV format
RGB Color Wheel Disable Get0x8A0x140x24Status code + RGB color wheel disable2Send when RGB color wheel to be disabled. 0x01 → color wheel disabled
Sensor DataSensor IDParameterParameter Length (Byte)Description
RGB LED On/Off status0x8A0x40On/Off status1RGB LED On/Off Status
Temperature data0x8A0x41Temperature sensor data2Temperature value in Celsius with 0.1 resolution. The MSB bit will be set when the negative temperature is reported
RGB LED Color data0x8A0x42RGB LED color data3RGB color value

Control Command Request and Response

The Control command request is used by mobile app to send the command to device. The control request channel is opened only after Client Characteristic Configuration Descriptor of TRS Ctrl Pt Characteristic notification is enabled; it is closed when such notification is disabled.

The format of Control command is an 8bit Opcode, an 8bit request ID followed by optional control payload.

Format of Control Command

ItemOp CodeLengthControl Request IDControl Payload
Size (Octet)111Variable

The control response is used by the device to send feedback to mobile app. The format of Response is an 8bit Opcode, an 8bit response ID and response status followed by optional Response payload.

Format of Control Response Data

ItemOp CodeLengthControl Response IDStatusControl Response Payload
Size (Octet)1111Variable

Status code 0x00 means successful execution of control command. Any status code other than 0x00 means error code, as shown in below Table. An error status does not have optional control Response payload.

Definition of Status Code

Status CodeDefinitionDescription
0x00SuccessResponse for successful operation
0x01Op Code Not SupportedResponse if unsupported Op Code is received
0x02Invalid ParameterResponse if Parameter received does not meet the requirements of the service.
0x03Operation FailResponse for fail operation
0x04-0xFFReserved for Future use

Sensor Notify Data

The Sensor data is sent to mobile app periodically by PIC32WM-BZ6204UE device. The sensor data channel is opened only after Client Characteristic Configuration Descriptor of TRS Ctrl Pt notification is enabled; it is closed when such notification is disabled.

The format of sensor data is an 8bit Opcode, an 8bit Sensor ID followed by sensor data payload.

Format of Sensor Data

ItemOp CodeLengthSensor IDSensor Payload
Size (Octet)111Variable