17.1 Steps for Porting an MCC Project from the PIC32WM_BZ6204 Module to the PIC32CX2051BZ66048 SoC and PIC32WM_BZ6602 Module

The following steps describe the complete procedure for migrating an existing PIC32WM_BZ6204 module project to the PIC32CX2051BZ66048 SoC and PIC32WM_BZ6602 module. The same migration steps apply to both targets.

  1. Launch the MPLAB® X IDE tool.
    Tip: The user must ensure to download and install the latest version of MPLAB X IDE Tool. The latest version ensures compatibility with Microchip devices and tools, allowing the user to develop for the newest hardware without issues. To download the latest version of the MPLAB X IDE tool, go to MPLAB® X IDE.
  2. In the opening window of the MPLAB X IDE, locate and open the PIC32WM_BZ6204 module application intended for migration.
  3. Open the project properties option in MPLAB X IDE.
    1. From the “Set Project Configuration” drop-down list, select Customize.
      Figure 17-1. Customizing the PIC32CX2051BZ66048 Project Properties
  4. In the Project Properties window, update the device configuration:
    1. The user must update the device name. From the “Device:” field drop-down list, select PIC32CX2051BZ66048.
      Note: For PIC32WM_BZ6602 module-based designs, select PIC32WM_BZ6602 from the Device: drop-down list instead of PIC32CX2051BZ66048.
    2. From the “Packs:” section, choose the latest version of the Device Family Pack (DFP). Expand the “PIC32CX-BZ6_DFP” folder, select 1.3.38.
      Note: The user must select the suggested DFP version (1.3.38 or latest).
    3. The user must choose the latest CMSIS version. Under “Packs:” section, expand the “CMSIS” folder, select 6.2.0.
    4. The user must select the recommended compiler version. From the “Compiler Toolchain:” section, expand “XC32 [Download Latest]” field, select XC32 (v4.60 or latest) [C:\Program Files\Microchip\xc32\v4.60\bin]. To download the latest version of the MPLAB XC32 compiler, got to MPLAB® XC32 Compiler.
    5. Click Apply, then click OK to ensure successful implementation of the configuration adjustments.
      Figure 17-2. Project Properties – Configuring Device, DFP, CMSIS and XC32 Compiler
  5. Navigate to the application configuration directory to verify the bsp folder. For example, go to H3\wireless_apps_pic32_bz6\apps\ble\advanced_applications\ble_ancs_app\firmware\src\config\default.
    Note:
    • If the bsp folder is not available, skip this step and proceed directly to step 7.
  6. If the bsp folder is available, perform the following steps:
    1. To generate the project graph, follow steps 7 through 12.
    2. After generating the project graph, the user must remove the BSP Component.
    3. To remove the bsp component, perform the following steps:
      1. Select the BSP Component.
        Figure 17-3. Selecting BSP Component
      2. Press Delete on the keyboard.
      3. The following pop-up appears to provide confirmation about deactivating the BSP component.
        Figure 17-4. Removing Module(s) Confirmation
      4. Click Yes to continue.
    4. The user must generate the project to reflect the PIC32CX2051BZ66048 SoC device change. For more details on project generation, follow steps 13 through 15.
      Note: For PIC32WM_BZ6602 migration, this step reflects the device change to the PIC32WM_BZ6602 module.
    5. After completing the project generation, the user must verify if the device name is updated or not in the definitions.h file.
      Note: For PIC32WM_BZ6602 migration, verify that DEVICE_NAME reflects PIC32WM_BZ6602 in the definitions.h file after project generation
      Figure 17-5. PIC32CX2051BZ66048 SoC – Device Name Update
      1. If the device name is not updated, follow these steps:
        Figure 17-6. PIC32CX2051BZ66048 SoC – Device Name Not Updated
      2. The user must close the Merge [MCC] tab.
      3. The “Question” pop-up appears and the user must click Yes to continue.
        Figure 17-7. Question – Closing Merge [MCC] Tab
      4. The user must close the MCC tab. The following pop-up appears and the user must click YES.
        Figure 17-8. MCC Alert – Closing MCC Tab
      5. The user must reopen MCC and regenerate the MCC project. To regenerate the MCC project, the user must perform steps 7 through 9.
      6. After completing the regeneration, the user must verify the regenerated project graph in the MCC tab.
        Figure 17-9. Regenerated Project Graph
      7. As the pin configuration differs between the PIC32WM_BZ6204 module and the PIC32CX2051BZ66048 SoC, update the pin assignments to match the PIC32CX2051BZ66048 SoC pinout in any application that uses these features (RGB LED, user buttons and LEDs).
        Table 17-1. PIC32CX2051BZ66048 SoC – RGB LED and User Buttons Configuration
        Pin NameCustom NameFunctionDirectionLatch
        RB7USER_LEDGPIOOutHigh
        RB9SWITCH1GPIOIn—
        RA4User buttonGPIOIn—
        RB3RGB_LED_GREENGPIOOutLow
        RB0RGB_LED_REDGPIOOutLow
        RB5RGB_LED_BLUEGPIOOutLow
      8. From the “Plugins:” drop-down list, select Pin Configuration.
        Figure 17-10. Project Graph – Pin Configuration Settings
      9. For example, in the Pin Settings tab, the user must perform the following steps:
        1. In the “Pin ID” column, go to RB3 pin.
        2. In the “Function” column drop-down list, select GPIO.
        3. In the “Direction (TRIS)” column, click and change it to Out.
        4. In the “Latch (LAT)” column, click and change it to Low.
        5. In the “Custom Name” column, change the name to RGB_LED_GREEN.
          Figure 17-11. PIC32CX2051BZ66048 SoC – Configuring RB3 GPIO Pin
          Note: This example shows how to configure the RB3 GPIO pin. The user must follow these steps to configure other pins of the PIC32CX2051BZ66048 SoC.
    6. After the user completes configuring the pins of the PIC32CX2051BZ66048 SoC, the user must proceed to regenerate the project. For regeneration, follow steps 13 through 21.
      Note: If the user encounters any build errors related to pin configurations, the user must manually update the pin details by clicking on the respective error in the Output tab. For manually updating the pin configurations, see Table 17-1.
  7. Run the Microchip Code Configurator (MCC) to begin the code configuration process.
    1. In the MPLAB X IDE opening window, click MCC.
      Figure 17-12. MPLAB X IDE Code Configurator (MCC)
    2. The following pop-up appears about the MCC core update. The user must update the core version to the latest version. To proceed with the update, click Yes.
      Figure 17-13. MCC Version Switching Confirmation
    3. The user must provide confirmation about device name switching. To proceed with the device name switching, click Yes.
      Figure 17-14. Device Name Switching Confirmation
  8. When the “Initializing project” pop-up appears, the user must wait for the initialization process to complete.
    Figure 17-15. MCC – Initializing Project
  9. The MCC now generates the project graph and the user can view it in the Project Graph tab.
    Note: The user must wait until the MCC generates the project graph.
    Figure 17-16. Project Graph
  10. The user clicks on the Device Family Pack (DFP) from the project graph to see the DFP for the selected device.
    1. The user must click the Device Family Pack (DFP) to open the DFP configuration window.
    2. In the DFP configuration window, the user must expand the “Device Family Pack (DFP)” entry to display the version information.
    Figure 17-17. DFP Confirmation
  11. The user verifies the package version, which is an essential step in ensuring that the correct version is utilized. To accomplish this, the user must perform the following steps:
    1. Click on the Device Resources tab to access the content manager.
    2. Click on the Content Manager (button at the top-right of the Device Resources tab) to access the content manager configuration options.
      Figure 17-18. Device Resources Tab and Content Manager
    3. The “Device” drop-down field allows the user to verify the type of device. In this scenario, it must be PIC32CX2051BZ66048.
      Note: For PIC32WM_BZ6602 migration, this field must show PIC32WM_BZ6602
    4. The “Content Type” drop-down field allows the user to verify the content type. In this scenario, it must be HARMONY.
      Figure 17-19. Device and Content Type Verification
    5. To locate and select the appropriate package version for the PIC32CX2051BZ66048 SoC, follow these steps for each applicable package using the “Search” field:
      1. Locate the package using the “Search” field.
      2. For example, type bsp in the search bar and press Enter on the keyboard.
      3. The user must select the latest version of the “bsp” package. For example, select v3.24.0 or latest from the “Version” column drop-down list.
        Figure 17-20. Search bsp, Select bsp and Select Version
        Important: Repeat this process for all applicable packages of the PIC32CX2051BZ66048 SoC. For more details on the applicable packages, see Applicable Harmony Packages – PIC32CX2051BZ66048 SoC table.
      The following table lists all the applicable harmony packages of the PIC32CX2051BZ66048 SoC and PIC32WM_BZ6602 module.
      Table 17-2. Applicable Harmony Packages
      ModuleVersions
      Corev3.16.0 or latest
      CSPv3.25.0 or latest
      BSPv3.24.0 or latest
      FreeRTOS-KernelV11.1.0(1)
      harmony-servicesV1.5.0 or latest
      wireless_blev1.5.0 or latest
      wireless_pic32cxbz_wbzv1.6.0 or latest
      wireless_system_pic32cxbz_wbzv1.8.1 or latest
      wireless_15_4_phyv1.4.0 or latest
      wireless_15_4_macv1.2.0 or latest
      openthreadmchp_harmony_wireless_thread_v1.3.0 or latest
      CMSIS_55.9.0 or latest
      touchV3.20.0 or latest
      Wireless_threadv1.3.0 or latest
      Note:
      1. The user must ensure to use the correct version for the FreeRTOS-Kernel package. For more details, go to wireless_apps_pic32_bz6/package.yml.
    6. Click Apply to continue.
      Figure 17-21. Applying the Changes
    7. After clicking Apply, wait for MCC to complete the update:
      1. Observe the “Download In Progress” pop-up notification.
        Figure 17-22. Package Download in Progress
      2. Observe the “Download Complete” pop-up notification.
        Figure 17-23. Package Download Complete
  12. After the package download completes, the “Loading...” pop-up appears, and the user must wait for the process to complete.
    Figure 17-24. Loading and Updating Project Content
  13. The user must perform a force update on all components. The following are the steps to perform a force update:
    1. In the Resource Management [MCC] tab, under the “Project Resources” field, right-click on the Generate, then click Force Update on All.
      Figure 17-25. Force Update on All Components
    2. Click Generate to start the process.
      Figure 17-26. Generating the Project
  14. When the “MCC Generating” pop-up appears, the user must wait for the initialization process to complete.
    Figure 17-27. MCC Generating
  15. After generating the code, the MCC initiates a merging process. The merging process is not going to make changes to the application files containing customized code. However, some applications do not require certain mergers.
    Note: The merging process does not modify any application files with names beginning with app_ and does not merge the user modified files like FreeRtos_hook.c file, and more.
  16. The user must thoroughly check to ensure the generation process is complete.
    Figure 17-28. Project Generation Complete
  17. The user must resolve the merge conflicts and build the project. When MCC detects differences in generated files, the MPLAB X IDE opens Merge [MCC] tab. The Merge [MCC] tab displays two panes within the Graphical tab:
    • MCC Updated Code: Generated (left pane): The newly generated output.
    • Merge Result: (right pane): The file MPLAB X IDE saves after the merge.
      Figure 17-29. MCC Updated Code: Generated and Merge Result: Pane
  18. The following are the different types of merge conflicts:
    • Type A: Replace device identifiers/specifications. The user must click the light-blue arrow “(→)” in a highlighted block to update the “MCC Updated Code: Generated” change into the “Merge Result:” file. For example, replace the PIC32WM_BZ6204 module with the PIC32CX2051BZ66048 SoC.
      Figure 17-30. Type A Merge Conflict Example
    • Type B: Remove unsupported functionalities that are highlighted in red color for the PIC32CX2051BZ66048 SoC. The user must click the “×” to remove the highlighted content from the “Merge Result:” file.
      Figure 17-31. Type B Merge Conflict Example
  19. The following are the steps to apply the merge changes:
    1. The user must confirm the file name in the merge title bar. For example, “Merge Result: definitions.h”.
    2. The user must scroll to each highlighted difference in the file and take action as per the requirement.
    3. For each highlighted difference, the user must take the required action:
      • For type A, the user must click the blue arrow (→) to replace the change. For more details on merge conflict types, see Step 17.
      • For type B, the user must click the red (×) to remove the change. For more details on merge conflict types, see Step 17
      Important: The user must repeat this process for each file displayed in the Merge [MCC] tab.
  20. The user must review the highlighted differences in each file that the Merge [MCC] tab shows and apply replace (→) or remove (×) action as per the requirement. For more details, see Step 17 and Step 18.
    Note: The following figures provide example references of merge conflict scenarios in common project source and header files. The user must scroll through each file thoroughly and resolve all highlighted differences by applying replace (→) or remove (×) action as applicable.
    • The following figure illustrates the merge conflicts scenarios in the definitions.h header file.
      Figure 17-32. Device Name Switching from PIC32WM_BZ6204 Module to PIC32CX2051BZ66048 (48L) SoC
    • The following figures illustrate the merge conflict scenarios in the device_vectors.h header file.
      Figure 17-33. SERCOM4 Peripheral Not Supported for PIC32CX2051BZ66048 (48L) SoC
      Figure 17-34. Ethernet Peripheral Not Supported for PIC32CX2051BZ66048 (48L) SoC
    • The following figure illustrates the merge conflicts scenarios in the plib_gpio.h header file.
      Figure 17-35. GPIO Port Pins Not Supported for PIC32CX2051BZ66048 (48L) SoC
    • The following figure illustrates the merge conflicts scenarios in the initialization.c source file.
      Figure 17-36. Ethernet and USB VBUS Peripheral Not Supported for PIC32CX2051BZ66048 (48L) SoC
      Figure 17-37. USB Peripheral Not Supported for PIC32CX2051BZ66048 (48L) SoC
    • The following figure illustrates the merge conflicts scenarios in the plib_clk.c source file.
      Figure 17-38. USB Power-Down UPLL Peripheral Not Supported for PIC32CX2051BZ66048 (48L) SoC
  21. Clean and build the main application, ensuring that the build is successful. From the drop-down list, click Clean and Build Main Project.
    Figure 17-39. Clean and Build Main Project
    Figure 17-40. Clean and Build Main Project – Build Successful
    1. The user must follow these steps to resolve any build errors:
      1. The user must click Clean and Build Main Project to build the project.
      2. If the build process reports errors, the user must locate the errors in the Output tab.
        Figure 17-41. PMD Registers – SERCOM4 Not Supported for PIC32CX2051BZ66048 (48L) SoC
      3. The user must select an error entry to navigate to the referenced file and line.
      4. The user must remove the unsupported code section that causes the error. Press Delete on the keyboard.
        Figure 17-42. PMD Registers – Deleting SERCOM4 Peripheral Not Supported
        Note: SERCOM4 is not supported on the PIC32CX2051BZ66048 (48L) SoC and PIC32WM_BZ6602 module devices. Therefore, remove the SERCOM4 peripheral from the PMD register configuration.
      5. The user must repeat steps ii to iv for each reported error.
      6. After resolving all reported errors, the user must click Clean and Build Main Project again.
      7. The user must look for BUILD SUCCESSFUL message in the Output tab.
        Note: This example shows one unsupported-functionality error scenario in one particular package. The user must follow the same steps to remove other unsupported functionality that causes build errors for the PIC32CX2051BZ66048 SoC.

Known Issue

After selecting the device in Project Properties and launching MCC for the first time, the DFP component in the Project Graph may continue to display the previously selected device name.

To update the DFP section with the correct device name, close MCC and reopen it. Launching MCC a second time refreshes the Project Graph and correctly updates the selected device information.