5.2.1.3 BLE Scanning Extended Advertisements

This section explains the scanning of Extended Advertisements (ADV_EXT_IND, ADV_AUX_IND) on the PIC32 BZ6 Curiosity board. For a successful scan of Extended Advertisement user needs to have a broadcaster transmitting these Advertisements. In BLE, a central or observer always starts with scanning.

Using the “scan_ext_adv” application example in combination with “ext_adv” example will enable users to test features like long range (Coded PHY) and sending data (1M, 2M, Coded PHY) over extended advertisements

Users can choose to either run the precompiled Application Example hex file provided on the PIC32 BZ6 Curiosity Board or follow the steps to develop the application from scratch.

It is recommended to follow the examples in sequence to understand the basic concepts before progressing to the advanced topics.

Hardware Requirement

Table 5-3. Hardware Prerequisites
S. No. Tool Quantity
1PIC32 BZ6 Curiosity Board2
2Micro USB cable2

SDK Setup

Refer to Getting Started with Software Development from Related Links.

Software Requirement

To install Tera Term tool, refer to the Tera Term web page in Reference Documentation from Related Links.

Smart phone App

None

Programming the Precompiled Hex File or Application Example

Using MPLAB® X IPE:

  1. Central Device – Import and program the precompiled hex file: <Discover Path>\wireless_apps_pic32_bz6\apps\ble\building_blocks\central\scan_ext_adv\precompiled_hex\scan_ext_adv.X.production.signed.hex.
  2. Peripheral Device – Import and program the precompiled hex file: <Discover Path>\wireless_apps_pic32_bz6\apps\ble\building_blocks\peripheral\ext_adv\precompiled_hex\ext_adv.X.production.signed.hex.
  3. For detailed steps, refer to Programming a Device in MPLAB® IPE in Reference Documentation from Related Links.
    Note: Ensure to choose the correct Device and Tool information.

Using MPLAB® X IDE:

  1. Perform the following the steps mentioned in Running a Precompiled Example. For more information, refer to Running a Precompiled Application Example from Related Links.
  2. Central Device – Open and program the application scan_ext_adv.X located in <Discover Path>\wireless_apps_pic32_bz6\apps\ble\building_blocks\central\scan_ext_adv\firmware.
  3. Peripheral Device – Open and program the application ext_adv.X located in <<Discover Path>\wireless_apps_pic32_bz6\apps\ble\building_blocks\peripheral\ext_adv\firmware.
  4. For more details on how to find the Discover path, refer to Download Application Example from Discover in Running a Precompiled Application Example from Related Links.

Demo Description

This application example enables users to do scanning of extended advertisements (ADV_EXT_IND, ADV_AUX_IND PDU's). Scanning of CODED PHY (125 kbps) is enabled by default in the application. After programming the application example, on Reset “ExtAdv Scan Enable Success” will be printed in the terminal window and if there is a broadcaster sending extended advertisements the Blue LED will toggle. If this broadcaster is another PIC32WM-BZ6204UE module programmed with “ext_adv.X” example it will print the application data sent in auxiliary packet - ADV_AUX_IND on TeraTerm. Toggling of Blue LED denotes the reception of extended advertisements.

Tera Term Configuration
  • Baud Rate/Speed – 115200 (as configured in SERCOM configuration)
  • Parity – None
  • Data Bits – 8
  • Stop Bits – 1
  • Flow Control – None

Testing

Users must use another PIC32 BZ6 Curiosity board configured as BLE Extended Advertisements, see BLE Extended Advertisements from Related Links.

This section assumes that a user has already programmed the ext_adv and scan_ext_adv application on two PIC32 BZ6 Curiosity boards.

  1. Board 1 – PIC32 BZ6 Curiosity board programmed with Ext Adv.
    1. Open TeraTerm and configure as mentioned below:
      Terminal Settings
      • Baud Rate/Speed – 115200 (as configured in SERCOM configuration)
      • Parity – None
      • Data Bits – 8
      • Stop Bits – 1
      • Flow Control – None
    2. Reset the board, Upon reset, “Ext Adv Enable” message is displayed on the TeraTerm.
  2. Board 2 – PIC32 BZ6 Curiosity Board Programmed with Scan Ext Adv.
    1. Open TeraTerm and configure as mentioned below:
      Terminal Settings
      • Baud Rate/Speed – 115200 (as configured in SERCOM configuration)
      • Parity – None
      • Data Bits – 8
      • Stop Bits – 1
      • Flow Control – None
    2. Reset the board. Upon reset, “ExtAdv Scan Enable Success” message is displayed on the TeraTerm.
    3. ext_adv scan will output all the extended advertisement and display the device name with MAC address will be displayed as soon the PIC32WM-BZ6204UE module performs an extended advertisement scan.

Blue LED is toggled when the observer device receives these extended advertisements. Sometimes, the PIC32CX BZ6 device appears twice simultaneously on Tera Term. During this time, the User LED toggles rapidly, indicating no actual toggle occurred.

Figure 5-19. Tera Term

Developing the Application from Scratch using MCC

Follow the steps below to build the application manually:
Note: It is recommended for the new users of the MPLAB Code Configurator to refer MPLAB® Code Configurator (MCC) User’s Guide in Reference Documentation from Related Links.
  1. Create a new harmony project. For more details, see Creating a New MCC Harmony Project from Related Links.
  2. Import component configuration – This step helps users setup the basic components and configuration required to develop this application. The imported file is of format .mc4 and is located in the path <Discover Path>\wireless_apps_pic32_bz6\apps\ble\building_blocks\central\scan_ext_adv\firmware\scan_ext_adv.X\.
    Note: Import and export functionality of component configuration will help users to start from a known working setup of configuration.
  3. Accept dependencies or satisfiers when prompted.
  4. Verify if the project graph window has all the expected configuration.
    Figure 5-20. Project Graph

Verifying Scan Configuration

  1. Click on the BLE_Stack component in project graph, to open component configuration and configure as illustrated in the following figure.
    Figure 5-21. BLE Stack Configuration

Files and Routines Automatically Generated by the MCC

After generating the program source from MCC interface by clicking Generate Code, the BLE configuration can be found in the following project directories
Figure 5-22. Project Files
Initialization routines for OSAL, RF System, and BLE System are auto-generated by the MCC. See OSAL Libraries Help in Reference Documentation from Related Links. Initialization routine executed during program initialization can be found in the project file.C.
Figure 5-23. initialization.c
The BLE stack initialization routine excuted during application initialization can be found in project files. This initialization routine is automatically generated by the MCC. This call initializes and configures the GAP, GATT, SMP, L2CAP and BLE middleware layers.
Figure 5-24. app_ble.c

Configuration for scanning extended advertisements is autogenerated

Autogenerated, Advertisement Data Format
Table 5-4. Source Files
Source FilesUsage
app.cApplication State machine, includes calls for Initialization of all BLE stack (GAP,GATT, SMP, L2CAP) related component configurations

app_ble\app_ble.c

Source Code for the BLE stack related component configurations, code related to function calls from app.c

app_ble\app_ble_handler.c

GAP, GATT, SMP and L2CAP Event handlers
app_user_edits.cUser code change instruction
Note: app.c is auto generated and has a state machine based application code sample. Users can use this template to develop their application.

Header Files

  • ble_gap.h(Header Files\config\default\ble\lib\include\) - This header file contains BLE GAP functions and is automatically included in the app.c file

Function Calls

MCC generates and adds the code to initialize the BLE Stack GAP, GATT, L2CAP and SMP in APP_BleStackInit() function

  • APP_BleStackInit() is the API that will be called inside the applications initial state APP_STATE_INIT in app.c

User Application Development

Include

  • Include the user action. For more information, refer to User Action from Related Links.
  • definitions.h in all the files where UART will be used to print debug information
Note: definitions.h is not specific to just UART peripheral, instead it must be included in all application source files where peripheral functionality will be exercised

Enabling Scanning of Extended Advertisement

  • BLE_GAP_SetExtScanningEnable (BLE_GAP_SCAN_MODE_OBSERVER, &extScan);

API's mentioned in this section are called in the Applications initial state - APP_STATE_INIT in app.c
// Enable Scanning the Ext Adv
uint16_t ret;
BLE_GAP_ExtScanningEnable_T extScan;
extScan.duration = 0x0;
extScan.enable = true;
extScan.filterDuplicates = BLE_GAP_SCAN_FD_ENABLE;
extScan.period = 0x0000;
ret = BLE_GAP_SetExtScanningEnable(BLE_GAP_SCAN_MODE_OBSERVER, &extScan );
if (ret == MBA_RES_SUCCESS)
       SERCOM0_USART_Write((uint8_t *)"ExtAdv Scan Enable Success\r\n", 28);
Figure 5-25. app.c

Configuring LED

Open the “Pin Configuration”
Verify the following Pin Settings

Scanning Results

  • The APP_Adv_Parser() function is used to extract the device name and the APP_HexToAscii() function is used to print the device name in a readable form. The code for the functions is below:

    uint8_t APP_Adv_Parser(uint8_t type, uint8_t* advData, uint8_t advLen, uint8_t* dataBuf)
    {
        // pointing to the first byte of advData
        uint8_t i=1;
        
        if(advLen<=1)
            return 0;
        
        for(; i< advLen; i += advData[i-1] + 1)
        {
            if(advData[i] == type)
                break;
        }
        
        if((i>= advLen)||                    // Cannot find the AD type
           (i + advData[i-1] - 1 > advLen))  // Check the data integrity 
            return 0;
            
        // data point to the AD data
        memcpy(dataBuf, advData+i+1, advData[i-1]-1);
        
        // return the AD length
        return advData[i-1]-1;
    }
    
    void APP_HexToAscii(uint8_t byteNum, uint8_t *p_hex, uint8_t *p_ascii)
    {
        uint8_t i, j, c;
        uint8_t digitNum = byteNum * 2;
    
        if (p_hex == NULL || p_ascii == NULL)
            return;
    
        for (i = 0; i < digitNum; i++)
        {
            j = i / 2;
            c = p_hex[j] & 0x0F;
    
            if (c >= 0x00 && c <= 0x09)
            {
                p_ascii[digitNum - i - 1] = c + 0x30;
            }
            else if (c >= 0x0A && c <= 0x0F)
            {
                p_ascii[digitNum - i - 1] = c - 0x0A + 'A';
            }
    
            p_hex[j] /= 16;
        }
    }
  • BLE_GAP_EVT_EXT_ADV_REPORT event is generated upon finding advertisements on legacy channels
// code snippet to print ext adv data
   uint8_t adLen, adContent[BLE_GAP_ADV_MAX_LENGTH];
 uint8_t printLen, printBuf[50];
// GPIO will toggle if it can scan any EXT ADV PDU
 USER_LED_Toggle();
 memset(adContent, 0 , BLE_GAP_ADV_MAX_LENGTH);
 memset(printBuf, 0, sizeof(printBuf));
 printLen = 0;
 // Check the advertisement if it contains Complete name field
 adLen= APP_Adv_Parser(0x09, p_event->eventField.evtExtAdvReport.advData,
 p_event->eventField.evtExtAdvReport.length, adContent);
 //Found
 if(adLen)
 {
 // Print out the Complete name
 memcpy(printBuf, adContent, adLen);
 printLen = adLen;
printBuf[printLen++] = ' ';
// Print out the BD address
APP_HexToAscii(GAP_MAX_BD_ADDRESS_LEN,p_event->eventField.evtAdvReport.addr.addr, printBuf+printLen);
printLen+=GAP_MAX_BD_ADDRESS_LEN*2;

printBuf[printLen++] = '\r';
printBuf[printLen++] = '\n';
SERCOM0_USART_Write(printBuf, printLen);                                        

}
Figure 5-26. app_ble_handler.c
Note: Users can explore more BLE Advertisement functionalities using the BLE Stack APIs. For more information, refer to BLE Stack in Reference Documentation from Related Links.

Where to Go from Here

See Central Devices from Related Links.