8.1.2 FFD Project Verification
LED indications :
In the coordinator if the blue LED in RGB LED glows the coordinator is powered ON and ready.
In the FFD the following are the different LED combinations indicating the following activity:
- Quick Green Flash of the RGB LED indicates the reception of data from the end device.
- Quick Blue Flash of User LED indicates that queued data was sent from coordinator to end device.
Following logs is the output generated by the coordinator in the Push Pull Star application.