5.2.2.6 BLE Transparent UART
This section explains how to create a peripheral device and send/receive characters between two connected BLE devices over Microchip proprietary Transparent UART Profile. Peripheral device will be the PIC32 BZ6 Curiosity board and central device can either be a Smart phone with Light Blue app or another PIC32 BZ6 Curiosity board.
Users can choose to either run the precompiled Application Example hex file provided on the PIC32 BZ6 Curiosity Board or follow the steps to develop the application from scratch.
It is recommended to follow the examples in sequence to understand the basic concepts before progressing to the advanced topics.
Recommended Readings
-
Getting Started with Application Building Blocks – See Building Block Examples from Related Links.
-
Getting Started with Peripheral Building Blocks – See Peripheral Devices from Related Links.
- See BLE Transparent UART from Related Links.
- See BLE Connection from Related Links
-
BLE Software Specification – See MPLAB® Harmony Wireless BLE in Reference Documentation from Related Links.
Hardware Requirement
| S. No. | Tool | Quantity |
|---|---|---|
| 1 | PIC32 BZ6 Curiosity Board | 1 |
| 2 | Micro USB cable | 1 |
| 3 | Android/iOS Smart phone | 1 |
SDK Setup
Refer to Getting Started with Software Development from Related Links.
Software Requirement
To install Tera Term tool, refer to the Tera Term web page in Reference Documentation from Related Links.
Smart phone App
Light Blue iOS/Android app available in stores
Programming the Precompiled Hex File or Application Example
Using MPLAB® X IPE:
- Import and program the precompiled hex
file:
<Discover Path>\wireless_apps_pic32_bz6\apps\ble\building_blocks\peripheral\profiles_services\peripheral_trp_uart\precompiled_hex\peripheral_trp_uart.X.production.signed.hex. - For detailed steps, refer to
Programming a Device in MPLAB® IPE in Reference
Documentation from Related Links.Note: Ensure to choose the correct Device and Tool information.
Using MPLAB® X IDE:
- Perform the following the steps mentioned in Running a Precompiled Example. For more information, refer to Running a Precompiled Application Example from Related Links.
- Open and program the application
peripheral_trp_uart.Xlocated in<Discover Path>\wireless_apps_pic32_bz6\apps\ble\building_blocks\peripheral\profiles_services\peripheral_trp_uart\firmware\peripheral_trp_uart.X. -
For more details on how to find the Discover path, refer to Download Application Example from Discover in Running a Precompiled Application Example from Related Links.
Demo Description
This application enables users to send data back and forth over UART between two connected BLE devices. On Reset, demo application prints “Advertising” which denotes the start of advertisements and then “Connected” when connection is established. Application data to be sent to the connected central device (smart phone or another PIC32 BZ6 Curiosity board) is entered in a terminal emulator like Tera Term. Data inputted in TeraTerm will be buffered and sent every 500 ms to allow for different data communication behavior. Input data accumulated within the 500 ms will be sent in a single BLE packet.
Testing
- Using a Micro USB cable, connect the Debug USB on the Curiosity board to a PC. The Active LED turns Green once connected to the PC.
- Program the precompiled hex file or application example as mentioned.
- Open TeraTerm and configure as mentioned
below:Terminal Settings:For more details on how to set the “Serial Port” and “Speed”, refer to COM Port Setup in Running a Precompiled Application Example from Related Links.
- Baud Rate/Speed – 115200 (as configured in SERCOM configuration)
- Parity – None
- Data Bits – 8
- Stop Bits – 1
- Flow Control – None
- Press the NMCLR button on the Curiosity board.
- Launch the Light Blue mobile app and
search for the device name “pic32cx-bz6” and press Connect. Users with an iOS
device may see the device name as “Microchip”.
Figure 5-90. LightBlue® App - To receive data from the PIC32 BZ6 Curiosity board (peripheral device) to the mobile app
(central device), select “UUID: 49535343-1E4D-4BD9-BA61-23C647249616” then select
Subscribe.
Figure 5-91. LightBlue® App Figure 5-92. LightBlue® App - Change the Data format to UTF-8 String in
the Light Blue mobile app then enter “test” on Tera Term. The same data must be displayed
in the app.Note: User may not be able to see “test” on the Tera Term as user types.
Figure 5-93. LightBlue® App - To send data from the mobile app (central
device) to the PIC32 BZ6 Curiosity board (peripheral device),
select “UUID: 49535343-8841-43F4-A8D4-ECBE34729BB3”.
Figure 5-94. LightBlue® App - Change the Data format to UTF-8
String then enter “trp uart” and click Write. The same data must be
displayed in Tera Term (see the following figure). Note: Data inputted in TeraTerm will be buffered and sent every 500 ms. Input data accumulated within the 500 ms will be sent in a single BLE packet.
Figure 5-95. LightBlue® App Note: Users can use another PIC32 BZ6 Curiosity board configured as BLE Transparent UART (central) instead of using a mobile app. For more information, refer to BLE Transparent UART from Related Links.
Developing the Application from Scratch using MCC
- Create a new harmony project. For more details, see Creating a New MCC Harmony Project from Related Links.
- Import component configuration – This
step helps users setup the basic components and configuration required to develop this
application. The imported file is of format
.mc4and is located in the path<Discover Path>\wireless_apps_pic32_bz6\apps\ble\building_blocks\peripheral\profiles_services\peripheral_trp_uart\firmware\peripheral_trp_uart.Note: Import and export functionality of Harmony component configuration will help users to start from a known working setup of MCC configuration. - Accept dependencies or satisfiers when prompted.
- Verify if the project graph window has
all the expected configuration. Note: Ensure that the macro
configUSE_TICKLESS_IDLEis set to0. The macro is available inFreeRTOSConfig.hfile#define configUSE_TICKLESS_IDLE 0
Verifying Advertisement,Connection and Transparent UART Profile Configuration
-
Select BLE Stack component in project graph, to open component configuration and configure as illustrated in the following figure.
Figure 5-97. BLE Stack Configuration - Select Transparent Profile component in project graph, to open component configuration and configure as illustrated in the following figure.
Generating a Code
For more details on code generation, refer to MPLAB Code Configurator (MCC) Code Generation from Related Links.
Files and Routines Automatically Generated by the MCC
initialization.capp_ble.c| Source Files | Usage |
|---|---|
app.c | Application State machine, includes calls for Initialization of all BLE stack (GAP,GATT, SMP, L2CAP) related component configurations |
app_ble\app_ble.c | Source code for the BLE stack related component configurations, code related to function
calls from app.c |
app_ble\app_ble_handler.c | GAP, GATT, SMP and L2CAP event handlers |
app_ble\app_trsps_handler.c | All transparent UART server related event handlers |
ble_trsps.c | All transparent server functions for user application |
app.c is autogenerated and has a state machine
based application code. Users can use this template to develop their own application.Header Files
ble_gap.h: Contains BLE GAP functions and is automatically included in theapp.cfile.ble_trsps.h: is associated with APIs and structures related to BLE Transparent Client functions for application user.
Function Calls
- MCC generates and adds the code to initialize the BLE Stack GAP, GATT, SMP and L2CAP in
APP_BleStackInit()function. APP_BleStackInit()is the API that will be called inside the Applications Initial State --APP_STATE_INITinapp.c.
User Application Development
Include
- Include the user action. For more information, refer to User Action from Related Links.
ble_trsps.hinapp.c, BLE Transparent UART Server related APIs.osal/osal_freertos_extend.hinapp_trsps_handler.c, OSAL related APIs are available here.definitions.hmust be included in all the files where UART will be used to print debug information.Note:definitions.his not specific to UART but instead must be included in all the application source files where any peripheral functionality will be exercised.
Set Public Device Address in app_ble.c
BLE_GAP_SetDeviceAddr(&devAddr);
BLE_GAP_Addr_T devAddr;
devAddr.addrType = BLE_GAP_ADDR_TYPE_PUBLIC;
devAddr.addr[0] = 0xA1;
devAddr.addr[1] = 0xA2;
devAddr.addr[2] = 0xA3;
devAddr.addr[3] = 0xA4;
devAddr.addr[4] = 0xA5;
devAddr.addr[5] = 0xA6;
// Configure device address
BLE_GAP_SetDeviceAddr(&devAddr);
app_ble.cStarting Advertisement
BLE_GAP_SetAdvEnable(0x01, 0x00);Figure 5-103. app.c
Connected and Disconnected Events
In
app_ble_handler.c,BLE_GAP_EVT_CONNECTEDevent will be generated when a BLE connection is completed
Connection Handler
- Connection handle associated with the peer peripheral device needs to be saved for data exchange after a BLE connection
p_event->eventField.evtConnect.connHandlehas this informationFigure 5-104. app_ble_handler.c
Transmit Data
-
Add “
APP_MSG_UART_CB” and “APP_TIMER_SEND_UART_MSG” to the generatedAPP_MsgID_T.Figure 5-105. app.h BLE_TRSPS_SendData(conn_hdl , 1, &data);is the API to be used for sending data to the central device.Note: The precompiled application example uses a UART callback to initiate the data transmission upon receiving a character in UART.-
Example for transmitting over UART using the
BLE_TRSPS_SendData()API
#define UART_DATA_MAX 25
uint16_t conn_hdl;// connection handle info captured @BLE_GAP_EVT_CONNECTED event
uint16_t ret;
uint8_t uart_data;
uint8_t uartBuf[UART_DATA_MAX];
uint8_t uartBufNum;
void uart_cb(SERCOM_USART_EVENT event, uintptr_t context)
{
APP_Msg_T appMsg;
// If RX data from UART reached threshold (previously set to 1)
if( event == SERCOM_USART_EVENT_READ_THRESHOLD_REACHED )
{
// Read 1 byte data from UART
SERCOM0_USART_Read(&uart_data, 1);
appMsg.msgId = APP_MSG_UART_CB;
OSAL_QUEUE_Send(&appData.appQueue, &appMsg, 0);
}
}
void APP_SendUartData()
{
// Send the uartBuf to connected device through Transparent service
if(uartBufNum == 0)
return;
BLE_TRSPS_SendData(conn_hdl, uartBufNum, uartBuf);
memset(uartBuf, 0 , sizeof(uartBuf));
uartBufNum = 0;
}
void APP_UartCBHandler()
{
uartBuf[uartBufNum] = uart_data;
if(++uartBufNum == UART_DATA_MAX)
{
APP_TIMER_StopTimer(APP_TIMER_SEND_UART);
APP_SendUartData();
}
else
APP_TIMER_SetTimer(APP_TIMER_SEND_UART,APP_TIMER_500MS, false);
}
// Enable UART Read
SERCOM0_USART_ReadNotificationEnable(true, true);
// Set UART RX notification threshold to be 1
SERCOM0_USART_ReadThresholdSet(1);
// Register the UART RX callback function
SERCOM0_USART_ReadCallbackRegister(uart_cb, (uintptr_t)NULL);
APP_BleStackInit();
// Start Advertisement
BLE_GAP_SetAdvEnable(0x01, 0x00);
// Reset the uart buffer
memset(uartBuf, 0, sizeof(uartBuf));
uartBufNum = 0;
SERCOM0_USART_Write((uint8_t *)"Advertising\r\n",13);
app.capp.celse if(p_appMsg->msgId==APP_MSG_UART_CB)
{
// Pass BLE UART Data transmission target BLE UART Device handling
APP_UartCBHandler();
}
else if(p_appMsg->msgId== APP_TIMER_SEND_UART_MSG)
{
APP_SendUartData();
} app.cReceive Data
BLE_TRSPS_EVT_RECEIVE_DATAis the event generated when data is sent from the central device- Use the
BLE_TRSPS_GetDataLength(p_event->eventField.onReceiveData.connHandle, &data_len);API to extract the length of the application data received BLE_TRSPS_GetData(p_event->eventField.onReceiveData.connHandle, data);API is used to retrieve the dataNote:BLE_TRSPS_Event_T p_eventstructure stores the information about BLE transparent UART callback functions.- Example for printing the received data from the central device over UART
/* TODO: implement your application code.*/
uint16_t data_len;
uint8_t *data;
// Retrieve received data length
BLE_TRSPS_GetDataLength(p_event->eventField.onReceiveData.connHandle, &data_len);
// Allocate memory according to data length
data = OSAL_Malloc(data_len);
if(data == NULL)
break;
// Retrieve received data
BLE_TRSPS_GetData(p_event->eventField.onReceiveData.connHandle, data);
// Output received data to UART
SERCOM0_USART_Write(data, data_len);
// Free memory
OSAL_Free(data);
app_trsps_handler.cWhere to go from Here
- BLE Sensor App – This application utilizes the Transparent UART building block, see BLE Sensor from Related Links.